Hello. We are trying to work with the DA14531 processor. When we open projects via KEil, we encounter the following problem. How can we solve this problem? Can you support?
No Algorithm found for: 07FC0000H - 07FC00A7H
Error: Flash Download failed - "Cortex-M0+"
Hi ylmaz,
Thank you for posting your questions online.
DA14531 could not support downloading to flash by keil.
You can program the flash by SmartSnippets Toolbox: 16. Flash Programming — DA145XX Tutorial SDK Getting started (renesas.com)
Any further questions are welcome.
BR,
JH_Renesas
Hi,Did you solve this issue? I am facing the same problem when I try to follow the Renesas tutorial for the first application. I found that the program can't be downloaded to flash using Keil; however, debugging might work as pointed out in the tutorial (I guess it's using RAM for debugging).
Hi There,Thank you for posting your question online.If you are facing the exact same issue as shown in the original post, please go on Options for Target -->UtilitiesThen you should be able to click on the Run Debug button to attach the debugger and download the firmware into the SRAM.For SPI Flash programming you will have to use our Development Tools:SmartBond Development Tools | RenesasPS: If you have any further questions, please raise a new ticket.Best Regards,OV_Renesas