Hello,
I am trying to develop code with DA14531. There are development environments with Keil, smart snippet and e2studio. I will not use Keil because it cannot write to flash. I successfully opened and uploaded the prox_reporter code in E2 studio. I could not open the other sample codes. How do I open the other codes? How do I upload the code? How do I develop the code? Can you direct me to the relevant resources to be faster?
lpccs-docs.renesas.com/.../migrating.html
I found the link above. Here it also says that I need to delete DA14531. How can I upload it for DA14531? I would be very happy if you could share the initial documentation to speed up my work. The project is urgent.
Thank you. Have a nice day.
Hi There,Thank you for posting your question online.For DA14531, Keil IDE is highly suggested since it has all the available examples. You are right you cannot write to the Flash directly with Keil, but you can use the SmartBond Flash Programmer | Renesas.e2 Studio IDE and SmartSnippets Toolbox IDE only have support for limited examples for the DA14531.You can either work directly on the prox_reporter example and built your application there or switch to Keil IDE.Best Regards,OV_Renesas