I do not need the full BLE stack on the DA14531. Is it possible to use the RF transmitter as a generic radio to support custom protocol such as Nordic's ShockBurst for example?
Hi Quang,
Thank you for posting your questions online.
Sorry it is not possible by now, some Stack are in the rom of DA14531.
By the way, what is your application scenario, we have SPS: UM-B-088: DA1453x/DA1458x Serial Port Service Reference Application (renesas.com)
BR,
JH_Renesas
I am trying to send 8 bytes packages at a fixed frequency of 100Hz. From my test, BLE protocol overhead limits the frequency to around 66Hz. I saw other chips from other manufacturers that support their own proprietary protocol. Those can just send arbitrary RF signals. I was hoping that DA14531 can do it as well.