DA14530 Booting from 2-wird UART not SPI slave issue.

Currently on a customized board, the DA14530 needs to be enabled via 2-wired UART.
But when I do the REST PING action, RX only receives 0x00 and not 0x02. Why is this?

There was originally a flash on the customized board but it has been removed. Will this have any impact?
My EVB board is normal.

Parents Reply Children