Currently on a customized board, the DA14530 needs to be enabled via 2-wired UART.But when I do the REST PING action, RX only receives 0x00 and not 0x02. Why is this?
There was originally a flash on the customized board but it has been removed. Will this have any impact?My EVB board is normal.
Hi There,Thank you for the reply.
00u18c18kvkwzgwmH358 said:Is P0_0 of default and picture supposed to be high or low instead after first power-on?
It should be high while the ROM Bootloader is running.Best Regards,OV_Renesas
Hi Thank you for the reply.
I've submitted an issue.Ticket: 393829.Please help push it. Thank you.