Hello Sir,
I am working with two DA14531 Tiny modules: one acting as a central and the other as a multi-com peripheral. After making changes as per the README file to support connecting to 3 devices, both modules initially connect. However, after 2-4 seconds, the central module automatically disconnects, and I receive the following error in the UART log: user_on_disconnect: reason: 08 (SMP_ERROR_CMD_NOT_SUPPORTED).
user_on_disconnect: reason: 08 (SMP_ERROR_CMD_NOT_SUPPORTED)
Hi Amar,The error you are facing is related to the Security configurations.My guess would be that you have enabled Security on the Peripheral side and that Central cannot access the Services without having a secure connection.Please check the Security configurations in order to make sure that both devices have either enabled or disabled security at the same time.Please refer here: DA1453x Tutorial BLE Security — DA1453x&DA1458x Tutorial BLE security (renesas.com)Best Regards,OV_Renesas
I am trying to send some data to a connected peripheral device through UART. I have reviewed the UART functionality in the peripheral example, but I am unsure of how to send data in the central code. Could you please guide me on how to implement the data transmission in the central device code?
Hi Amar,Thank you for the reply.Please refer on the following:(1) DA14531mod central request data - Bluetooth Low Energy - Wireless Connectivity - Renesas Engineering CommunityOn this thread I had explained the Central related APis on how to Read/Write on the Peripheral characteristics.(1) DA14531 Central With Security Read Characteristic - Bluetooth Low Energy - Wireless Connectivity - Renesas Engineering CommunityPlease share more information regarding the Application Scenario and what is the expected the behavior of your application so we can actually guide you.Best Regards,OV_Renesas
Hi Amar,Please also check this thread as well:(1) DA14531 central device with multiple characteristic UUID - Bluetooth Low Energy - Wireless Connectivity - Renesas Engineering CommunityBest Regards,OV_Renesas
Hello sir,
I hope you're doing well. I am currently working on storing data in a variable through UART communication on the central device (DA14531). However, I'm encountering an issue where I am unable to store the data correctly.
HI Amar,Thank you for the reply.I hope you are doing well too.Could you please share more information? A high level description of your application scenario and the code snippets of what you are trying to achieve?Best Regards,OV_Renesas
I hope you're doing well. am working with two DA14531 Bluetooth modules (Central and Multi-Com Peripheral) to send data via the GATT write function using UART. The communication works fine when the Mobile Bluetooth LightBlue app is used as the central device, but when using the DA14531 as the central device, the write operation fails after approximately 40-50 seconds, returning error code 0045, indicating a failure in the GATTC_WRITE process.
0045
GATTC_WRITE
the central device output on COM
Completion Event: GATTC_DISC_ALL_SVC: status: 00001235Received data: 0x31 0x32 0x33 0x35 check string to integer convert is =1235GATTC_WRITE: status: 0000Write successful!
1543Received data: 0x31 0x35 0x34 0x33 check string to integer convert is =1543GATTC_WRITE: status: 0045Write failed, status: 0045
1000Received data: 0x31 0x30 0x30 0x30 check string to integer convert is =1000GATTC_WRITE: status: 0043Write failed, status: 0043
Hi Amar,Thank you for the reply.The errors you are facing are:
///Request not allowed in current state. GAP_ERR_COMMAND_DISALLOWED = 0x43, ///Requested operation timeout. GAP_ERR_TIMEOUT = 0x45,
OV_Renesas said:Do you have Security implemented?
I have disable sleep mod function
static const sleep_state_t app_default_sleep_mode = ARCH_SLEEP_OFF;
OV_Renesas said:Could you please share the Full Service Discovery information?
static void handle_svc_ind(uint8_t con_idx, struct gattc_sdp_svc_ind const *disc_svc) { service_info_t *svc = ke_malloc(user_ble_get_svc_size(disc_svc), KE_MEM_NON_RETENTION); if (svc == NULL) { dbg_block_printf("Error: Service allocation failed\r\n",NULL); return; } dbg_block_printf("%s: conn_idx=%04x start_h=%04x end_h=%04x\r\n", __func__, con_idx, disc_svc->start_hdl, disc_svc->end_hdl); user_gatt_parse_service(disc_svc, svc, con_idx); uint16_t i; dbg_block_printf("%s: check gatt_char_handle =%04x\r\n",gatt_char_handle); #ifdef ENABLE_IAS bool ias_uuid_match; uint16_t ias_uuid = ATT_SVC_IMMEDIATE_ALERT; uint16_t ias_alert_uuid = ATT_CHAR_ALERT_LEVEL; if(svc->svc_uuid.type == ATT_UUID_16){ ias_uuid_match = match_uuid((uint8_t *)&ias_uuid, (uint8_t *)&svc->svc_uuid.uuid.uuid16, sizeof(uint16_t)); } if(ias_uuid_match){ dbg_block_printf("Immediate Alert Service: ", NULL); } #endif #ifdef ENABLE_BAS bool bas_uuid_match; uint16_t bas_uuid = ATT_SVC_BATTERY_SERVICE; uint16_t bas_level_uuid= ATT_CHAR_BATTERY_LEVEL; if(svc->svc_uuid.type == ATT_UUID_16){ bas_uuid_match = match_uuid((uint8_t *)&bas_uuid, (uint8_t *)&svc->svc_uuid.uuid.uuid16, sizeof(uint16_t)); } if(bas_uuid_match){ dbg_block_printf("Battery Service: ", NULL); } #endif dbg_block_printf("%s: \r\n", format_uuid(&svc->svc_uuid) ); for(i = 0 ; i<svc->num_chars; i++) { gattc_chars_t *gatt_char = &svc->items[i]; #ifdef ENABLE_IAS if(ias_uuid_match) { if( match_uuid( (uint8_t *)&ias_alert_uuid , (uint8_t *)&gatt_char->uuid.uuid, 2) ) { memcpy(¢ral_app_env.periph_devices[con_idx].serv_disc.ias_char, gatt_char, sizeof(gattc_chars_t) ); central_app_env.periph_devices[con_idx].serv_disc.ias_handle_valid = true; dbg_block_printf("\tAlert Level Char\r\n", NULL); if(gatt_char->c.properties & GATT_PROP_WRITE) { central_app_env.periph_devices[con_idx].serv_disc.ias_write_op = GATTC_WRITE; } else if(gatt_char->c.properties & GATT_PROP_WRITE_NO_RESP) { central_app_env.periph_devices[con_idx].serv_disc.ias_write_op = GATTC_WRITE_NO_RESPONSE; } else if(gatt_char->c.properties & GATT_PROP_WRITE_SIGNED) { central_app_env.periph_devices[con_idx].serv_disc.ias_write_op = GATTC_WRITE_SIGNED; }else { central_app_env.periph_devices[con_idx].serv_disc.ias_handle_valid = false; } } } #endif #ifdef ENABLE_BAS if(bas_uuid_match) { if( match_uuid( (uint8_t *)&bas_level_uuid , (uint8_t *)&gatt_char->uuid.uuid, 2) ) { memcpy(¢ral_app_env.periph_devices[con_idx].serv_disc.bas_char, gatt_char, sizeof(gattc_chars_t)); central_app_env.periph_devices[con_idx].serv_disc.bas_handle_valid = true; dbg_block_printf("\tBattery Level Char\r\n", NULL); } } #endif dbg_block_printf("\t%04x char %s prop=%02x (%s)\r\n", gatt_char->handle, format_uuid(&gatt_char->uuid), gatt_char->c.properties, format_properties(gatt_char->c.properties)); } ke_free(svc); central_app_env.periph_devices[con_idx].serv_disc.last_handle = disc_svc->end_hdl; }
"I have made some changes in the user_central_app_c file. I have taken input data from the user through UART and sent the data to the peripheral device."
user_central_app_c
#define SCAN_INTVL_MS (50) #define SCAN_WINDOW_MS (50) #define HANDLE 0x0025 timer_hnd uart_receive_timer_used __SECTION_ZERO("retention_mem_area0"); static void uart_receive_cb(uint16_t length); void continuous_uart_send_callback(); void send_data_to_peripheral(); typedef struct { struct bd_addr addr; }connecting_device_t; typedef struct { periph_device_t periph_devices[CFG_MAX_CONNECTIONS]; bool connect_to_periph; struct bd_addr connect_to_addr; uint8_t connect_to_addr_type; uint8_t num_connections; timer_hnd connection_timer; }central_app_env_t; central_app_env_t central_app_env; /* * FUNCTION DEFINITIONS **************************************************************************************** */ #define UART_RECEIVE_BUFFER_SIZE 4 uint8_t uart_receive_buffer[UART_RECEIVE_BUFFER_SIZE]; volatile bool uart_receive_finished = false; volatile uint16_t data_received_cnt = 0; //Data sent via UART will be stored here uint8_t received_data[UART_RECEIVE_BUFFER_SIZE] = {0}; void uart_receive_interrupt_example(uart_t* uart) { uart_receive_finished = false; data_received_cnt = 0; uart_register_rx_cb(uart, uart_receive_cb); uart_receive(uart, uart_receive_buffer, UART_RECEIVE_BUFFER_SIZE, UART_OP_INTR); uart_receive_timer_used = app_easy_timer(300, continuous_uart_send_callback); } uint8_t con_idx = 0; uint16_t gatt_char_handle = 0x002c ; static void uart_receive_cb(uint16_t length){ uart_receive_finished = true; data_received_cnt = length; //Copy uart_receive_buffer data to received_data memcpy(&received_data,uart_receive_buffer , sizeof(uart_receive_buffer)); uart_receive_timer_used = app_easy_timer(300, continuous_uart_send_callback); // Null-terminate the string if it's textual received_data[length] = 0; // Debug the received data dbg_block_printf("Received data: ",NULL); for (int i = 0; i < data_received_cnt; i++) { dbg_block_printf("0x%02X ", received_data[i]); } dbg_block_printf("\r\n",NULL); wdg_resume(); // Re-enable the Extended Sleep Mode // arch_set_extended_sleep(false); // Re-enable the app_easy_timer if (uart_receive_timer_used != EASY_TIMER_INVALID_TIMER) { uart_receive_timer_used = EASY_TIMER_INVALID_TIMER; } // Handle the received data by sending it to the connected GATT characteristic send_data_to_peripheral(); } void send_data_to_peripheral() { // arch_set_extended_sleep(true); uint8_t con_idx = 0; // Connection index //uint8_t gatt_char_handle = 0x002c; // uint8_t gatt_char_handle = 0x0027; // Handle for the characteristic uint16_t num = 0; for(int i=0;i<sizeof(received_data);i++){ if(received_data[i]>='0' && received_data[i]<='9'){ num = num*10+(received_data[i]-'0'); } else { break; } } dbg_block_printf("check string to integer convert is =%d\r\n",num); dbg_block_printf(" Checking code with sleep mode function.... \r\n",NULL); arch_asm_delay_us(5); user_ble_gatt_write(GATTC_WRITE, con_idx, gatt_char_handle, &num, sizeof(num)); arch_asm_delay_us(5); } void continuous_uart_send_callback(){ // arch_disable_sleep(); uart_receive_interrupt_example(UART2); // Start UART reception }
OV_Renesas said:Could you please share the API you used to perform the GATTC_WRITE?
"I have to perform the GATT_Write function after user_gatt_discover_all_services in the user_on_connection function."
GATT_Write
user_gatt_discover_all_services
user_on_connection
void user_on_connection(uint8_t connection_idx, struct gapc_connection_req_ind const *param) { if(central_app_env.connection_timer != EASY_TIMER_INVALID_TIMER){ app_easy_timer_cancel(central_app_env.connection_timer); central_app_env.connection_timer = EASY_TIMER_INVALID_TIMER; } default_app_on_connection(connection_idx, param); dbg_printf("%s\r\n", __func__); central_app_env.periph_devices[connection_idx].addr = param->peer_addr; central_app_env.periph_devices[connection_idx].con_idx = connection_idx; central_app_env.periph_devices[connection_idx].con_valid = true; central_app_env.num_connections++; dbg_block_printf("Communicate with peripheral..... \r\n", NULL); dbg_printf("Connected to device with address: %02X:%02X:%02X:%02X:%02X:%02X\r\n", param->peer_addr.addr[5], param->peer_addr.addr[4], param->peer_addr.addr[3], param->peer_addr.addr[2], param->peer_addr.addr[1], param->peer_addr.addr[0]); if(central_app_env.num_connections < CFG_MAX_CONNECTIONS) { ble_scan_for_devices(); } #ifdef ENABLE_IAS central_app_env.periph_devices[connection_idx].serv_disc.ias_handle_valid = false; #endif #ifdef ENABLE_BAS central_app_env.periph_devices[connection_idx].serv_disc.bas_handle_valid = false; #endif user_gatt_discover_all_services(connection_idx, 1); uart_receive_timer_used = app_easy_timer(300, continuous_uart_send_callback); }
I have undefine security
#undef CFG_APP_SECURITY
Hi Amar,Thank you for the reply.Regarding the Full Service Discovery:I was referring on the Logs you have received on your terminal.On your send_data_to_peripheral function you are using the 0x002C Characteristic handler. I would like to see the Service and Characteristic permissions for this specific handler.I would also remove the arch_asm_delay_us API. Adding extra delays while you have a BLE connection established can lead to BLE mistimings and that would result in the BLE connection being terminated.Best Regards,OV_Renesas