DA14531 central disconnect issue

Hello Sir, 

I am working with two DA14531 Tiny modules: one acting as a central and the other as a multi-com peripheral. After making changes as per the README file to support connecting to 3 devices, both modules initially connect. However, after 2-4 seconds, the central module automatically disconnects, and I receive the following error in the UART log: user_on_disconnect: reason: 08 (SMP_ERROR_CMD_NOT_SUPPORTED).