Hi Ahmad,
What kind of second bootloader you want build?
Does this project can help which is in the SDK path:
DA145xx_SDK\6.0.22.1401\utilities\secondary_bootloader
BR,
JH_Renesas
Did you have tried with the latest SDK V6.0.22.
Please let me know if you done the test and is there any reason why you are still using the old SDK6.0.16
Hi JH Renesas,We haven't tried with the latest SDK V6.0.22 yet.We are currently facing issues with the ROM Bootloader. I am not sure if the latest sdk will resolve it.But I will test with the latest SDK and get back to you.It would also be good to know if we have any size limitations or which RAM sections can be overridden, and which should not be touched while loading? What's the maximum size in RAM our secondary bootloader can have?
Our team has following this question via email, thanks for your questions.