Hello,
I would like to generate a unique Bluetooth device address for a DA14531 chip that has the SPS SDK firmware. I changed the define USER_CFG_ADDRESS_MODE to APP_CFG_ADDR_STATIC in user_config.h file and got the following error when trying to build the hex file.
.\out_531\dsps_device_531.axf: Error: L6388E: ScatterAssert expression (ImageBase(RET_HEAP_MSG) + ImageLength(RET_HEAP_MSG) < (((0x7fc9c00) + (((((0x33e) + (((0x3 * 0x3) + (0x3 + 0x3)) * (0x106))) + ((0x8) * (0x106))) + (0x6)) - ((((0x33e) + (((0x8) + (((0x1))) + (0x3)) * ((((0xfb)) OR 0x1) + 0x4 + 0x7))) + ((0x8) * ((((0xfb)) OR 0x1) + 0x4 + 0x7))) + (0x6)))) AND (0xffffc00))) failed on line 153 : (0x7fc9c04 < 0x7fc9c00)
When the configuration is #define USER_CFG_ADDRESS_MODE APP_CFG_ADDR_PUB, I can successfully build without issues.
I am currently using a DA14531 USB dev kit. The current device address I am seeing on the SmartConsole App is from the following -
#define CFG_NVDS_TAG_BD_ADDRESS {0x02, 0x00, 0xF4, 0x35, 0x23, 0x48}
I could change this define to get a unique address but this would not be feasible solution in production where the same hex file will need to be loaded into all the products.
Thanks,
Lekha
Hi Lekha,
Thank you for posting your questions online.
Let me test in this and will back to you as soon as possible.
BR,
JH_Renesas
Hi Lekha,Please go on da14531_config_advanced.h file and reduce the MSG Heap size:
#define MSG_HEAP_SZ 3950 //(4 * 1024)
Thank you for your response. I am also able to build successfully after making this change. Thank you.