Hi Sir,
Help me to configure hibernation sleep mode in central code, my requirement is the device should scan for 10 seconds and the device should enter into Hibernation sleep, what are the changes I need to do in Central Code.
Note : I need to achieve datasheet Hibernation sleep current (270nA).
Hi Susmi,
Thank you for posting your questions online.
1, Are you using EVK or customer board?
2, Which example project you are using?
3, if it's customer board, which SPI flash you are using?
BR,
JH_Renesas
1. here i am using EVK board
2. in central code, i am trying to implement hibernation sleep
Could you check this tutorial for sleep mode, any further questions are welcome.
DA1453x & DA1458x Sleep Modes Tutorial — DA1453x & DA1458x Tutorial Sleep Modes (renesas.com)