Central Scan with Hibernation sleep

Hi Sir,

               Help me to configure hibernation sleep mode in central code, my requirement is the device should scan for 10 seconds and the device should enter into Hibernation sleep, what are the changes I need to do in Central Code.  

Note : I need to achieve datasheet Hibernation sleep current (270nA).

Parents Reply Children
No Data