Hibernation Sleep current in Scanning

Hi Sir,

 

        I have configured a hibernation sleep after scanning, i can able to achieve 26.2uA after Powering down the SPI flash, How to reduce the current consumption further.

        I have attached the code below

static void ble_scan_for_devices()
{

ke_state_set(TASK_APP, APP_CONNECTABLE);
ble_gap_error_t err = user_ble_gap_start_scan(true, SCAN_INTVL_MS, SCAN_WINDOW_MS, false);
dbg_block_printf("Started Scanning!!!!!!!!!!!!!!!!!!!\r\n", NULL);
ASSERT_ERROR(err == BLE_GAP_ERROR_NO_ERROR);
//app_easy_timer(200, scan_stop);
scan_timer=app_easy_timer(200, scan_stop);

}


void scan_stop(){
user_ble_gap_stop_scan();
dbg_block_printf("Stopped Scanning!!!!!!!!!!!!!!!!!!!\r\n", NULL);
// dbg_block_printf("Timer state before cancel: %d\r\n", scan_timer);
++timer;

SetBits16(PMU_CTRL_REG, TIM_SLEEP, 1);
// Wait until PD_TIM is closed
while ((GetWord16(SYS_STAT_REG) & TIM_IS_DOWN) != TIM_IS_DOWN);
// Power down the flash to reduce current consumption during Hibernation
spi_flash_power_down();
// spi_flash_ultra_deep_power_down();
//Enter Hibernation4
//time_result =++timer;
arch_set_hibernation(HIB_WAKE_UP_PIN_MASK,
PD_SYS_DOWN_RAM_OFF,
PD_SYS_DOWN_RAM_OFF,
PD_SYS_DOWN_RAM_OFF,
REMAP_ADDR0_TO_ROM,
false);
}