DA14541 USB Development Kit as Programmer: SWDIO & Reset

Good morning,

I am transitioning from the DA14531 USB Dev Kit to a custom prototype board. I was able to correctly configure the Dev Kit for programming per the serial wire debug guide. The custom prototype is now recognized by the Keil IDE and can enter debug mode.

However, when attempting to run the code there is an issue with CPU being halted which I believe is related to the reset line. Log below:

* JLink Info: Memory map 'after startup completion point' is active
* JLink Info: CPU could not be halted
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 16 (XPSR) while CPU is running
***JLink Error: Cannot read register 0 (R0) while CPU is running
***JLink Error: Cannot read register 1 (R1) while CPU is running
***JLink Error: Cannot read register 2 (R2) while CPU is running
***JLink Error: Cannot read register 3 (R3) while CPU is running
***JLink Error: Cannot read register 4 (R4) while CPU is running
***JLink Error: Cannot read register 5 (R5) while CPU is running
***JLink Error: Cannot read register 6 (R6) while CPU is running
***JLink Error: Cannot read register 7 (R7) while CPU is running
***JLink Error: Cannot read register 8 (R8) while CPU is running
***JLink Error: Cannot read register 9 (R9) while CPU is running
***JLink Error: Cannot read register 10 (R10) while CPU is running
***JLink Error: Cannot read register 11 (R11) while CPU is running
***JLink Error: Cannot read register 12 (R12) while CPU is running
***JLink Error: Cannot read register 13 (R13) while CPU is running
***JLink Error: Cannot read register 14 (R14) while CPU is running
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 16 (XPSR) while CPU is running
***JLink Error: Cannot read register 17 (MSP) while CPU is running
***JLink Error: Cannot read register 18 (PSP) while CPU is running
***JLink Error: Cannot read register 20 (CFBP) while CPU is running

My questions are:

1. Is this error likely due to the reset line being disconnected?

2. How do I connect BOTH the SWDIO pin AND Reset from my custom PCB to the USB dev kit given that the SWDIO connection (per serial wire debug guide) uses the connection labeled as RES on the actual silk layer of the USB dev kit?

*I currently have P0_0 multiplexed with UART_TX and Reset by using a resistor to for the connection. Only UART_TX was connected on the custom PCB.

Parents
  • Hi There,

    Thank you for posting your question online.
    I suppose you have followed the procedure shown here: 20. Serial Wire Debug Probe — DA145XX Tutorial SDK Getting started

    1. Is this error likely due to the reset line being disconnected?

    On your Keil project please go on Options for Target and on Utilities make sure you have selected the highlighted option:


    2. How do I connect BOTH the SWDIO pin AND Reset from my custom PCB to the USB dev kit given that the SWDIO connection (per serial wire debug guide) uses the connection labeled as RES on the actual silk layer of the USB dev kit?

    There is no need to connect Reset pin. You only need SWDIO, SWCLK, VBAT and GND.

    Best Regards,
    OV_Renesas

  • Awesome! Thank you so much for your response. I’ll give that a shot when I get back to my computer.

    Is it possible to enable UART as well? Does that work with the same DIP Switch configuration as the serial wire debug probe guide?

    EDIT: Unfortunately, that was not the issue. The Keil IDE was already correctly configured. After further research, I heard it may be due to clock speed with longer wires for SWDIO/SWCLK but it is set as low as 20 kHz with no luck. I've also confirmed I'm using a 32 MHz crystal oscillator as used by the dev kit. Are there any other common causes for this issue?

    Context with other settings below:


  • Hi Nate,

    Thank you for the reply.
    Could you please try to use SmartSnippets Toolbox and download your FW directly into RAM?
    We would like to verify that the custom board is working properly and then we can see why the debugger cannot be attached.
    You can get SmartSnippets Toolbox from here: SmartBondTm Development Tools | Renesas
    You can either use SWD or UART programming to download the FW into the SRAm.

    Best Regards,
    OV_Renesas

  • For some reason I am unable to reply to this answer. I have a loading icon at the bottom as shown:

  • HI Nate,

    Thank you for the reply.
    You can try to delete your browser cookies and try again.
    Did you try to load the FW into the SRAM?

    Best Regards,
    OV_Renesas

  • Good morning,

    I have tried attaching the logs as a file in the hopes that it allows the post to go through. I first attempted and failed to download to RAM. Then I realized I should select JTAG from the Board dropdown. It appeared to work. Lastly, I tried flashing the code for further debug information. All logs included.

    First attempt to Download firmware to RAM:
    
    [ACTION   General@25-03-13 20:17:19] Please press the hardware reset button on the board to start the download process.
    [INFO     General@25-03-13 20:17:21] Reset detected
    [INFO     General@25-03-13 20:17:24] UART port "COM6" has been opened.
    [INFO     General@25-03-13 20:17:29] UART port has been released.
    [INFO     Booter@25-03-13 20:18:47] Read 3704 bytes from file C:\Renesas\DA145xx_SDK\6.0.16.1144\projects\target_apps\peripheral_examples\blinky\Keil_5\out_DA14531\Objects\blinky_531.hex.
    [INFO     RAM@25-03-13 20:18:47] Connection to COM6 port has successfully opened.
    [INFO     RAM@25-03-13 20:18:47] Started download procedure...
    [ACTION   RAM@25-03-13 20:18:48] Please press the hardware reset button on the board to start the download process.
    [INFO     RAM@25-03-13 20:18:51] Reset detected
    [ERROR    RAM@25-03-13 20:18:51] CRC does not match.
    [ACTION   RAM@25-03-13 20:18:51] Please click the Connect/Download button in SmartSnippets Toolbox and press the hardware reset button on the board to start the download process.
    [INFO     Booter@25-03-13 20:18:51] Successfully disconnected from port COM6.
    [ERROR    RAM@25-03-13 20:18:51] Failed downloading Image file to the board.
    
    Second attempt to Download firmware to RAM (appeared successful after enabling JTAG from Board menu):
    
    [INFO     RAM@25-03-13 20:22:03] Found SW-DP with ID 0x0BC11477
    [INFO     RAM@25-03-13 20:22:03] DPIDR: 0x0BC11477
    [INFO     RAM@25-03-13 20:22:03] AP map detection skipped. Manually configured AP map found.
    [INFO     RAM@25-03-13 20:22:03] AP[0]: AHB-AP (IDR: Not set)
    [INFO     RAM@25-03-13 20:22:03] AP[0]: Core found
    [INFO     RAM@25-03-13 20:22:03] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     RAM@25-03-13 20:22:03] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     RAM@25-03-13 20:22:03] Found Cortex-M0 r0p1, Little endian.
    [INFO     RAM@25-03-13 20:22:03] FPUnit: 4 code (BP) slots and 0 literal slots
    [INFO     RAM@25-03-13 20:22:03] CoreSight components:
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0] @ E00FF000
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
    [INFO     RAM@25-03-13 20:22:03] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:03] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:03] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:03] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:04] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:04] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:04] Successfully downloaded Image file to the board.
    
    Attempted to Flash Code for further debug info:
    
    [INFO     Flash Code@25-03-13 20:24:06] Found SW-DP with ID 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] DPIDR: 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] AP map detection skipped. Manually configured AP map found.
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP (IDR: Not set)
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: Core found
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     Flash Code@25-03-13 20:24:06] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     Flash Code@25-03-13 20:24:06] Found Cortex-M0 r0p1, Little endian.
    [INFO     Flash Code@25-03-13 20:24:06] FPUnit: 4 code (BP) slots and 0 literal slots
    [INFO     Flash Code@25-03-13 20:24:06] CoreSight components:
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0] @ E00FF000
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: SYSRESETREQ has confused core.
    [INFO     Flash Code@25-03-13 20:24:06] Found SW-DP with ID 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] DPIDR: 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] AP map detection skipped. Manually configured AP map found.
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP (IDR: Not set)
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: Core found
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     Flash Code@25-03-13 20:24:06] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     Flash Code@25-03-13 20:24:06] Found Cortex-M0 r0p1, Little endian.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Using fallback: Reset pin.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via reset pin
    [INFO     Flash Code@25-03-13 20:24:06] Firmware File C:\Program Files\SmartSnippetsToolbox\SmartSnippetsToolbox5.0.24\common_resources\SupportPackages\DA1453x\toolbox_resources/common/jtag_programmer_531.bin has been selected for downloading.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [WARNING  SPI Flash Programmer@25-03-13 20:24:17] Failed configuring SPI ports and pins.
    [INFO     Flash Code@25-03-13 20:24:17] Successfully downloaded firmware file to the board.

Reply
  • Good morning,

    I have tried attaching the logs as a file in the hopes that it allows the post to go through. I first attempted and failed to download to RAM. Then I realized I should select JTAG from the Board dropdown. It appeared to work. Lastly, I tried flashing the code for further debug information. All logs included.

    First attempt to Download firmware to RAM:
    
    [ACTION   General@25-03-13 20:17:19] Please press the hardware reset button on the board to start the download process.
    [INFO     General@25-03-13 20:17:21] Reset detected
    [INFO     General@25-03-13 20:17:24] UART port "COM6" has been opened.
    [INFO     General@25-03-13 20:17:29] UART port has been released.
    [INFO     Booter@25-03-13 20:18:47] Read 3704 bytes from file C:\Renesas\DA145xx_SDK\6.0.16.1144\projects\target_apps\peripheral_examples\blinky\Keil_5\out_DA14531\Objects\blinky_531.hex.
    [INFO     RAM@25-03-13 20:18:47] Connection to COM6 port has successfully opened.
    [INFO     RAM@25-03-13 20:18:47] Started download procedure...
    [ACTION   RAM@25-03-13 20:18:48] Please press the hardware reset button on the board to start the download process.
    [INFO     RAM@25-03-13 20:18:51] Reset detected
    [ERROR    RAM@25-03-13 20:18:51] CRC does not match.
    [ACTION   RAM@25-03-13 20:18:51] Please click the Connect/Download button in SmartSnippets Toolbox and press the hardware reset button on the board to start the download process.
    [INFO     Booter@25-03-13 20:18:51] Successfully disconnected from port COM6.
    [ERROR    RAM@25-03-13 20:18:51] Failed downloading Image file to the board.
    
    Second attempt to Download firmware to RAM (appeared successful after enabling JTAG from Board menu):
    
    [INFO     RAM@25-03-13 20:22:03] Found SW-DP with ID 0x0BC11477
    [INFO     RAM@25-03-13 20:22:03] DPIDR: 0x0BC11477
    [INFO     RAM@25-03-13 20:22:03] AP map detection skipped. Manually configured AP map found.
    [INFO     RAM@25-03-13 20:22:03] AP[0]: AHB-AP (IDR: Not set)
    [INFO     RAM@25-03-13 20:22:03] AP[0]: Core found
    [INFO     RAM@25-03-13 20:22:03] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     RAM@25-03-13 20:22:03] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     RAM@25-03-13 20:22:03] Found Cortex-M0 r0p1, Little endian.
    [INFO     RAM@25-03-13 20:22:03] FPUnit: 4 code (BP) slots and 0 literal slots
    [INFO     RAM@25-03-13 20:22:03] CoreSight components:
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0] @ E00FF000
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
    [INFO     RAM@25-03-13 20:22:03] ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
    [INFO     RAM@25-03-13 20:22:03] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:03] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:03] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:03] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:04] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     RAM@25-03-13 20:22:04] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     RAM@25-03-13 20:22:04] Successfully downloaded Image file to the board.
    
    Attempted to Flash Code for further debug info:
    
    [INFO     Flash Code@25-03-13 20:24:06] Found SW-DP with ID 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] DPIDR: 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] AP map detection skipped. Manually configured AP map found.
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP (IDR: Not set)
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: Core found
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     Flash Code@25-03-13 20:24:06] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     Flash Code@25-03-13 20:24:06] Found Cortex-M0 r0p1, Little endian.
    [INFO     Flash Code@25-03-13 20:24:06] FPUnit: 4 code (BP) slots and 0 literal slots
    [INFO     Flash Code@25-03-13 20:24:06] CoreSight components:
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0] @ E00FF000
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT
    [INFO     Flash Code@25-03-13 20:24:06] ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: SYSRESETREQ has confused core.
    [INFO     Flash Code@25-03-13 20:24:06] Found SW-DP with ID 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] DPIDR: 0x0BC11477
    [INFO     Flash Code@25-03-13 20:24:06] AP map detection skipped. Manually configured AP map found.
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP (IDR: Not set)
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: Core found
    [INFO     Flash Code@25-03-13 20:24:06] AP[0]: AHB-AP ROM base: 0xE00FF000
    [INFO     Flash Code@25-03-13 20:24:06] CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    [INFO     Flash Code@25-03-13 20:24:06] Found Cortex-M0 r0p1, Little endian.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Using fallback: Reset pin.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via reset pin
    [INFO     Flash Code@25-03-13 20:24:06] Firmware File C:\Program Files\SmartSnippetsToolbox\SmartSnippetsToolbox5.0.24\common_resources\SupportPackages\DA1453x\toolbox_resources/common/jtag_programmer_531.bin has been selected for downloading.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Halt core after reset via DEMCR.VC_CORERESET.
    [INFO     Flash Code@25-03-13 20:24:06] Reset: Reset device via AIRCR.SYSRESETREQ.
    [WARNING  SPI Flash Programmer@25-03-13 20:24:17] Failed configuring SPI ports and pins.
    [INFO     Flash Code@25-03-13 20:24:17] Successfully downloaded firmware file to the board.

Children