Good morning,
I am transitioning from the DA14531 USB Dev Kit to a custom prototype board. I was able to correctly configure the Dev Kit for programming per the serial wire debug guide. The custom prototype is now recognized by the Keil IDE and can enter debug mode.
However, when attempting to run the code there is an issue with CPU being halted which I believe is related to the reset line. Log below:
* JLink Info: Memory map 'after startup completion point' is active* JLink Info: CPU could not be halted***JLink Error: Cannot read register 15 (R15) while CPU is running***JLink Error: Cannot read register 16 (XPSR) while CPU is running***JLink Error: Cannot read register 0 (R0) while CPU is running***JLink Error: Cannot read register 1 (R1) while CPU is running***JLink Error: Cannot read register 2 (R2) while CPU is running***JLink Error: Cannot read register 3 (R3) while CPU is running***JLink Error: Cannot read register 4 (R4) while CPU is running***JLink Error: Cannot read register 5 (R5) while CPU is running***JLink Error: Cannot read register 6 (R6) while CPU is running***JLink Error: Cannot read register 7 (R7) while CPU is running***JLink Error: Cannot read register 8 (R8) while CPU is running***JLink Error: Cannot read register 9 (R9) while CPU is running***JLink Error: Cannot read register 10 (R10) while CPU is running***JLink Error: Cannot read register 11 (R11) while CPU is running***JLink Error: Cannot read register 12 (R12) while CPU is running***JLink Error: Cannot read register 13 (R13) while CPU is running***JLink Error: Cannot read register 14 (R14) while CPU is running***JLink Error: Cannot read register 15 (R15) while CPU is running***JLink Error: Cannot read register 16 (XPSR) while CPU is running***JLink Error: Cannot read register 17 (MSP) while CPU is running***JLink Error: Cannot read register 18 (PSP) while CPU is running***JLink Error: Cannot read register 20 (CFBP) while CPU is running
My questions are:
1. Is this error likely due to the reset line being disconnected?
2. How do I connect BOTH the SWDIO pin AND Reset from my custom PCB to the USB dev kit given that the SWDIO connection (per serial wire debug guide) uses the connection labeled as RES on the actual silk layer of the USB dev kit?
*I currently have P0_0 multiplexed with UART_TX and Reset by using a resistor to for the connection. Only UART_TX was connected on the custom PCB.