Hello Dialog
I downloaded e2studio and successfully built SPS_6.150.8.83 and CODELESS_6.380.20.66 on DA14585
my questions are:
1. Is it possible to reduce the code size? when I try to change the optimization level from None (-O0) to Optimize size (-Oz), the image size still does not change (the default compiler is LLVM)
2. when I try to change the compiler to ARM Compiler 6.16, it fails to compile; can you provide the relevant settings that need to be configured?
Thanks
Robin