Hi There,
I use the sdk version is 6.0.22.1401. And I use the Bare_Bone case. I could scanned the device through the computer bluetooth, android system mobile phone bluetooth as well. But I couldn't sanned the device by iphone bluetooth. In addition to using the SmartBond APP on my iphone, I can't scan the device. So, I would like to ask a question that what is the reason for this situation?
Thanks for your assist!
BR,
NX
HI NX,Thank you for posting your question online.Are you sure you have enabled Bluetooth and Location on your SmartPhone in order to be able to scan for BLE devices?You are facing this issue only with ble_app_barebone example?Have you modified the Advertising configurations?Best Regards,OV_Renesas
Look this:
It's my Iphone Bluetooth info.
Thanks for your assits!
Hi NX,Thank you for the reply.
南瞎 said:For your First question: I'm preety sure I opened the Blutooth on my Iphone.
For BLE Devices the Location is mandatory as well.
南瞎 said:For your Second question: All of the ble examples.
That is strange. Are you working with an EVK or a custom board?Can you replicate this behavior with an EVK?Best Regards,OV_Renesas
Thanks for your answer.
I used the board designed by myself. For your second question, sorry, I can't.
For this case, I also feel stranging, I have tried to use various brands of mobile phone. Android system is fine. And there are three modes for create ad message, just ADV_IND mode can scan. And I use the medthod belongs to ADV_IND to create ad message. Is that right?
I have downloaded the SmartBone APP on my Iphone, and I haven't downloaded the SmartBone APP on my Android mobile phone. Is it possible that it has something with the SmartBone APP? For example, after Bluetooth is turned on, the APP first scans the device and then for some reason makes the iphone unable to scan the device. Just my guess! I'll test it tomorrow.
Hi NX,Thank you for the reply.Have you verified that your custom board works?Are you able to run any FW and see the device advertising?To me it sounds like a HW issue on your board.Best Regards,OV_Renesas
Look!
Hi NX,Thank you for the reply.Are you able to connect via your PC?Have you tried any other SmartPhones?The DA14531 is not detectable by any other device other than your PC?Best Regards,OV_Renesas
Thanks for your reply.
The third picture is show the PC situation.
For the issue, I had checked the website of Iphone, and I found some advise. And I did it. The issue was slove.
In addition, I would like to ask how to use Power Profile tool? And does it require certain conditions(tools and stuff)?
6.2. Power Profiler — UM-B-083 This link I had checked. But I couldn't use the Power Profile tool nomally. That mean is I couldn't started Power Profile tool.
Hi NX,Apologies for the delay.
南瞎 said:In addition, I would like to ask how to use Power Profile tool? And does it require certain conditions(tools and stuff)? 6.2. Power Profiler — UM-B-083 This link I had checked. But I couldn't use the Power Profile tool nomally. That mean is I couldn't started Power Profile tool.
The Power Profiler is only available with our Current Circuit which is included in our DA14531-00FXDEVKT-P - SmartBond TINY DA14531 Bluetooth Low Energy 5.1 System-on-Chip Development Kit Pro | RenesasPlease check UM-B-114: DA14531 Development Kit Pro Hardware User Manual, on section 8. Current Measurements.Best Regards,OV_Renesas