DA14592 BLE Notify Maximum 60 Bytes

Hello,

I have used BLE peripheral example ( custom service + asy ) as reference where i have addded two characteristics in which i want to exchange 256 bytes of data.

I am able to send  only 60 bytes of data to mobile application (tested nrf Connect for IOS) ,

That is in firmware i made a provision that when i receive a certain command from BLE application the firmware should reply with these 256 bytes of data,

but when i check this in application i get only 60 data.

So please help me soo that i can get this data correct and full in one shot,

I had changed the MTU size to 512 bytes, but nothing changed



Regards

Jc.

  • Hi There,

    Thank you for posting your question online.
    Could you please share your custom service?
    I would like to see the size of the Characteristic.
    You are trying to update (Notify) the value of this specific characteristic with 256 bytes?
    Could you please share that implementation as well?

    Best Regards,
    OV_renesas 

  • Hi JC,

    Apologies for the delay.
    I tried to replicate this on my side but I was not able.
    I used the Custom Service example from git: ble-sdk10-da1459x-examples/connectivity/ble_custom_service_example at main · renesas/ble-sdk10-da1459x-examples
    I made the following changes:

    /* Just to demonstrate how notifications can be sent explicitly for dedicated attribute handles */
    #define APP_NOTIF_DEMONSTRATION            ( 1 )
    
    /**
     * Attribute values maximum size expressed in bytes
     *
     * \warning The remote device must not exceed that number. Otherwise, the system will crash!!!
     *
     */
    #define ATTR_MAX_SIZE                      ( 260 )
    

    Then at the end of the ble_peripheral_task.c file where we Notify data on the characteristics:

    #if APP_NOTIF_DEMONSTRATION
                    /*
                     * The following code is just for demonstration purposes to illustrate how notifications
                     * can be sent explicitly for a specific attribute handle.
                     * A connected peer device will receive notifications/indications only if has them enabled
                     * explicitly. The notification type is defined automatically based on its associated
                     * attribute declaration.
                     */
                    if (notif & NOTIF_TIMER_EVENT) {
                            /* Generate a random number with the help of the TRNG engine */
                            int arbitrary_value = rand();
    
                            uint8_t test_val[256]= {0};
                            for (int i=0;i<256;i++){
                            	test_val[i] = rand();
                            }
    
                            /* Send notifications for a specific attribute value (referenced by its UUID) */
                            mcs_send_notifications(CHARACTERISTIC_ATTR_1_128_UUID,
                                 (const uint8_t *)&test_val, sizeof(test_val));
    
                            mcs_send_notifications(CHARACTERISTIC_ATTR_4_128_UUID,
                                 (const uint8_t *)&arbitrary_value, sizeof(arbitrary_value));
                    }
    #endif

    On my side it works as expected. I am able to see the Characteristic of the 1st Service being notified every 5 seconds with 256 random bytes.

    Best regards,
    OV_Renesas