DA14592 BLE Notify Maximum 60 Bytes

Hello,

I have used BLE peripheral example ( custom service + asy ) as reference where i have addded two characteristics in which i want to exchange 256 bytes of data.

I am able to send  only 60 bytes of data to mobile application (tested nrf Connect for IOS) ,

That is in firmware i made a provision that when i receive a certain command from BLE application the firmware should reply with these 256 bytes of data,

but when i check this in application i get only 60 data.

So please help me soo that i can get this data correct and full in one shot,

I had changed the MTU size to 512 bytes, but nothing changed



Regards

Jc.