Hello Renesas Community,
I'm currently working with the EK-RA6M4 evaluation kit and trying to interface it with the US159-DA14531EVZ. However, I'm having trouble getting the two boards to communicate or function together properly. Here is my previous question: Compatibility between RA0E1 Fast Prototyping Board and US159-DA14531EVZ Evaluation Board
I followed the exact same steps like this one, but it's not working. Here's my current setup:
In SmartBond, I’m seeing 'DLG-PROXR' instead of 'DA14531-FSP-BLE' as defined in QE for BLE. I'm not sure why this mismatch is happening.
Here is my project: BLE.rarAny help or recommendations would be greatly appreciated. Thank you in advance!