I am creating a new ticket since my replies to my previous ticket are not getting approved.
The current architecture is based off of 6.380.16.55. Would it be possible to introduce a circular pipe to send incoming stream of data (more than 251 byte) over BLE at 115200 baud rate or increase the byte handler max size? Trying to introduce anything above 251 breaks the BT connection (GATT operation failed for unknown reason).
I am working with set two standalone, not datapump. Does moving to datapump cause any issues with size constrains? Also, I need the following as well.
#define USE_AT_PWRLVL #define USE_AT_RSSI #define USE_AT_HRTBT #define USE_AT_CMD #if CMD_LOCAL_SOURCE==CMD_UART #define USE_AT_BAUD #endif
Could I enable them under user_at_commands.h for #if defined(USE_AT_BINARY_MODE)?