Continuous TX Carrier Mode & Channel Selection on Renesas BT Module (CodeLess / Custom Firmware)

We are working on RF measurements with a Bluetooth module from Renesas and need to configure the device for continuous TX carrier mode along with channel selection capabilities.

From our communication with Renesas, we understand:

  • There is no custom firmware developed for this purpose by Renesas.

  • The available firmware is CodeLess, which uses AT commands.

  • While transmission power can be adjusted using CodeLess, channel selection for TX carrier mode does not seem to be supported.

We would like to ask:

  1. Is there a developer version of the app or a dedicated PC software that can allow us to set the device into continuous TX carrier mode and select specific channels for testing?

  2. Is there any way to configure multiple channels or perform frequency hopping under a controlled test scenario?

  3. While we understand that transmission power can be adjusted using CodeLess, could someone please guide us on how exactly this is done?

We appreciate any insights or shared experiences on setting up the Renesas BT module for RF testing, especially continuous transmission and channel configuration.

Thanks in advance!

Parents Reply Children