SDK6 import issues with same sample project over different independent work spaces

I have noticed that if I open a completely new work space estudio remembers that a sample project has been imported earlier and denies an import in the new fresh workspace. 

That is not handy for upgrades which require the latest estudio and sdk like the current upgrade.

How is that issue be best addressed, a new SDK location for each independent project ?

Thanks

Ralph

update

It seems that this issue affects all sample projects even those I have not imported before.

I will try on a virgin machine to see if I can import according to the documentation.



seems a more general issue
[edited by: Rales at 17:18 (GMT 0) on 25 May 2025]
Parents Reply
  • Yes, of course. And it is even worse. On an absolute virgin machine I have this message on any project from the SDK even if it has not been used before.

    e-studio 25-4 latest from May 16. and SDK 6.0.24

    On my working machine I first updated e-studio via the update dialog. Then I uninstalled e-studio and deleted all files related to it. reinstalled, Problem remained.

    Urgent solution needed

Children