I have noticed that if I open a completely new work space estudio remembers that a sample project has been imported earlier and denies an import in the new fresh workspace.
That is not handy for upgrades which require the latest estudio and sdk like the current upgrade.
How is that issue be best addressed, a new SDK location for each independent project ?
Thanks
Ralph
update
It seems that this issue affects all sample projects even those I have not imported before.
I will try on a virgin machine to see if I can import according to the documentation.
Even when I completely uninstall estudio, delete all work spaces and reinstall estudio this problem remains
Hi Rales,
Thank you for posting your questions online.
Are you using this item to import the project?
BR,
JH_Renesas
Yes, of course. And it is even worse. On an absolute virgin machine I have this message on any project from the SDK even if it has not been used before.
e-studio 25-4 latest from May 16. and SDK 6.0.24
On my working machine I first updated e-studio via the update dialog. Then I uninstalled e-studio and deleted all files related to it. reinstalled, Problem remained.
Urgent solution needed
Could you please try the older version in the search bar type in e2studio 2025-01:
we will test if the latest version has bugs later.
What about the SDK then, in the documentation for the 6.0.24 it says that 25-4 is required.
This needs immediate investigation please, likely that is the cause
Could you try this selection instead
yes I did but leaves unresolved includes, even basic once like uint8 etc.
please make sure the path is correct, the git hub examples should be placed here:
I follow the instructions on Github and the cloning commant puts the repo here
and by the way trying to import any target_apps want to specify the compiler version while none are offered for selecting
any update? still working on?
what is the selection when you install the e2studio? details please find here:
1. Prerequisites — e2 Studio SDK 6 Getting Started Guide
Jason
I don't understand your answer as I explained this before here!
At first I updated via the e-studio/eclipse 'search for updates' menu. Then I cleaned the the machine for a fresh install of e-studio as shown in the video. All same result.
Can anybody replicate this issue?