I have noticed that if I open a completely new work space estudio remembers that a sample project has been imported earlier and denies an import in the new fresh workspace.
That is not handy for upgrades which require the latest estudio and sdk like the current upgrade.
How is that issue be best addressed, a new SDK location for each independent project ?
Thanks
Ralph
update
It seems that this issue affects all sample projects even those I have not imported before.
I will try on a virgin machine to see if I can import according to the documentation.
Even when I completely uninstall estudio, delete all work spaces and reinstall estudio this problem remains
> Even when I completely uninstall estudio, delete all work spaces and reinstall estudio this problem remains> Some projects had already been imported before.Project information is generated in .metadata folder and it prevents from importing the same name of project.It's workspace issue, so no need to re-install e² studio.Create a new folder and start e² studio with the folder as new workspace.Refer to this FAQ about project import.FAQ - e² studio project import is prevented by existing projectshttps://en-support.renesas.com/knowledgeBase/20630043
that is exactly what you expect and DOS NOT WORK LIKE YOU EXPECT so take my problem serious and consider that I do this job longer then you are existing on this planet.