SDK6 import issues with same sample project over different independent work spaces

I have noticed that if I open a completely new work space estudio remembers that a sample project has been imported earlier and denies an import in the new fresh workspace. 

That is not handy for upgrades which require the latest estudio and sdk like the current upgrade.

How is that issue be best addressed, a new SDK location for each independent project ?

Thanks

Ralph

update

It seems that this issue affects all sample projects even those I have not imported before.

I will try on a virgin machine to see if I can import according to the documentation.



seems a more general issue
[edited by: Rales at 17:18 (GMT 0) on 25 May 2025]
Parents Reply Children
  • Look, did you try to replicate the problem?

    Why you don't explain and look into why with with SDK 6.0.24 e-studio 25-4 is required?

    Will you answer if that is influencing the compatibility of using 6.0.22 with 25-4? seems logic

    I noticed the issue by opening a new workspace to generate a new flavor od the simple_beacon I worked on. Then I notices that I get the same message for ANY sample project I even never touched before.