Hello Renesas community,
I have two BLE variants
1) one should connect with authentication,
2) second it should connect without authentication,
But both should happen with same software, I can differentiate these scenario by using VCU signal.
When ever the mobile app asks for the parring code user_app_on_tk_exch this function will get called.
From this function I need to call the below function with the same parring code that send by mobile app(central).
app_easy_security_tk_exch(paring_conidx, (uint8_t*)&ble_passward,sizeof(ble_passward), true);
Any other way I can skip these authentication steps.
Thanks for the help you are providing.