Hi,
Somehow the thread " https://www.dialog-semiconductor.com/support-posts/da16200-mqtt-dpm " was bricked.
So opening this new one.
"""PM_Dialog
Hi Premsai,
According to our Team internally, we need some extra info regarding that issue. Please check below.
1. dpm status
2. mqtt configuration
Can you please share that screenshots from your side?
Regards,
PM_Dialog"""
Reply:
Since i'm not allowed to share confidential information some of the info are masked.Please find the snapshots.
Prem Sai
Hi Prem Sai,
DA16200 sends a packet every hour normally.
Regarding abnormal wakeup, DA16200 wakes up because of MQTT Disconnection - please check below :
In this case, DA16200 didn't receive response from AP.
--------------------------------------------------------------------------------------------------------------------
QUESTIONS
Q1 : Do you know if the host controls the power of DA16200 or not?
I can see 0x00, 0x04 and 0x82 as wakeup source.
0x00 : at+restart
0x04 : por reset
0x82 : wakeup by rtc timer.
Q2 : Are they using those wake up source?
If you are not using at+restart/por reset for DA16200, you can get the log as follow.
IMPORTANT NOTE :
Please describe your testing scenario, so that we can test it on our side.
Best regards,
PM_Dialog