Hi There,
didnt found the place where i can change the hostname of the Module.
Any document or file / function to watch for?
Thanks Tecomon
Hi ST-Kon,Please refer on the last answer on this ticket.Please check dhcp_option_hostname() function in dhcp.c file.
The name is CHIPSET_NAME_MACADDR[5:4] by default.
It is placed in "\core\libraries\3rdparty…
Hello PM_Dialog,
at the moment the hostname seems to be Dialog_ with the last hex digits of the mac address. This shows firstly the module used on the final product, and secondly no connection to the manufacturer of the final product. So someone will put it on their network, see a device "Dialog_123456" and not know what it is, and maybe block it since most end users don't open the devices.
Also, it could be that there are multiple products with the same hostname in this scenario.
Thanks, Tecomon