DA16200mod FreeRTOS 3.2.0.0 Hostname

Hi There,

 

didnt found the place where i can change the hostname of the Module. 

Any document or file / function to watch for?

 

Thanks Tecomon

Parents
  • Hi There,

    tested the code but without success.

    nvram_status was fine and didnt failed.

    zero_config task was running.

     

    Still the hostname appears as:

    DA16200_D29C (172.24.1.74) auf d4:3d:39:10:d2:9c [ether] auf wlan0
    Tested with and without clearing the nvram.

     

    Any idea how to debug or another way to set the hostname?

     

    Thanks, Tecomon

Reply
  • Hi There,

    tested the code but without success.

    nvram_status was fine and didnt failed.

    zero_config task was running.

     

    Still the hostname appears as:

    DA16200_D29C (172.24.1.74) auf d4:3d:39:10:d2:9c [ether] auf wlan0
    Tested with and without clearing the nvram.

     

    Any idea how to debug or another way to set the hostname?

     

    Thanks, Tecomon

Children
No Data