DA16200mod FreeRTOS 3.2.0.0 Hostname

Hi There,

 

didnt found the place where i can change the hostname of the Module. 

Any document or file / function to watch for?

 

Thanks Tecomon

Parents
  • Hi there,

     

    I am running into the same issue. I keep seeing DA16200-XXXX where XXXX stands for the last four digits of the mac address as the hostname whether or not i use zeroconfig.

     

    Device is running in STA mode. Goal is to not use zeroconfig and change the hostname that the device advertises into the local network.

     

    Logfile is attached but nothing to see regarding this issue and a screenshot from a networkscanner where you can see the default hostname.

    34489.zip
Reply
  • Hi there,

     

    I am running into the same issue. I keep seeing DA16200-XXXX where XXXX stands for the last four digits of the mac address as the hostname whether or not i use zeroconfig.

     

    Device is running in STA mode. Goal is to not use zeroconfig and change the hostname that the device advertises into the local network.

     

    Logfile is attached but nothing to see regarding this issue and a screenshot from a networkscanner where you can see the default hostname.

    34489.zip
Children
No Data