I have the DA16200 evaluation board. I am trying to connect to my AWS account. I have mqtt_config setup as shown below. when I try to connect I get the following message. It is crucial that I am able to connect to my AWS account using TLS and certificates. I have loaded the 3 certificates that I use to connect to my AWS account from other boards. These certificates work for all other cases.
/DA16200/NET] # cert #1 (MQTT, Enterprise) - Root CA: O - Certificate: O - Private Key: O - DH Parameter: X #2 (HTTPs, CoAPs Client) - Root CA: X - Certificate: X - Private Key: X - DH Parameter: X
mqtt_client_check_conn failed [mosquitto__socket_connect_tls] Failed to establish tls-sess(0x7200) [_mosquitto_socket_connect_step3] Failed to connect tls-sess(19) Unable to connect (TLS Handshake failed.) [SUB] REQ mqtt_restart (count=1)
MQTT Client Information: - MQTT Status : Not Running - Broker IP : xxx-ats.iot.us-east-1.amazonaws.com - Port : 8883 - Pub. Topic : da16k - Sub. Topic : da16ks - QoS Level : 1 - TLS : Enable - Ping Period : 600 - TLS Incoming buf : 4096(bytes) - TLS Outgoing buf : 4096(bytes) - TLS Auth mode : 1 - User name : <None> - Password : (None) - Client ID : test_id - MQTT VER : 3.1
Hi There,
Thanks for sharing the complete log file. We'll go through it. In the meantime, can you check if you can replicate it with our latest SDK release?
Thanks, PM_Dialog