I am attempting to load RTOS image #1 via the MROM.
loady 1e2000
do the ymodem stuff. seems to work.
Changed boot index to 1 (from RTOS #0). Reboot.
MROM indicates an error and drops to the command prompt:
Image Header, CRC Failed (b84c8891 - cfec6341) [0003d813]!!
This is ymodem at 234000 baud on the EVK board, so I'm not sure how there could possibly have been a bit error during the download. I have retried multiple times. No luck.
Can you change the boot index back to 0 from MROM? I do not see any documentation on how to do this.
Hi Jeremy,
Thanks for your question. Can you please reset it to factory defaults?
At the [/DA16200] prompt, type factory to do a factory reset.
Regards,
PM_Renesas
Hi
I'd like to add to this question
When I am trying to run from a corrupted image (CRC failed) the systems remains in MROM prompt so I only have mrom commands and 'factory' is not one of the options.
Beside reburning the image, is it possible to switch to the other RTOS image?
Thanks
Hi There,Could you please share more information?Which Wi-Fi chip are you using? Which SDK version are you using? Are you referring to any corrupted image from the ones we provide?Could you please share the full logs?It would be better if you raised a new ticket regarding your issue since this is an older one. Kind Regards,OV_Renesas
I opened a new ticket