RA2L1 DA16200 UNABLE TO COMUNICATE WITH AT COMMAND

Hy all, I have tryed to send and receive At command with DA16200 connected at PMOD2 of EK-RA2L1.

I think thaht the pin in "stack" configuration are correct but im not able to see nothing on uart response and teraterm not work.

this is thwe output that i receive on segger j link terminal

But "1F;" is a random word that i do not this is a response by the module DA16200.

Do you know a simple way to send to module "ATZ" and receive read a simple asnwer "OK" is very very frustrating?

There is a way to run this module with arduino code and just find an easy way to enstabilish a connection with wifi modem ?