"DM_RTC_WAKEUP" observed while DA16200MOD is already in sleep mode

Hi there,

I'm using DA16200MOD with AWS SDK version: DA16200_DA16600_SDK_v3.2.4.0_AWS_0 integrated in DA16200_DA16600_SDK_FreeRTOS_v3.2.4.0.

I have observed that when DA16200MOD is in sleep (SLEEP mode 3) with DPM settings (as below), device automatically wake-up after (approx. 20 mins).

DDPS Enable -NO

DPM Keep Alive Time- (Default 30000 ms)

DPM User Wakeup Time(0~86400 Sec.)- (Default 0 Sec.)

DPM TIM Wakeup Count(1~65535 dtim) - 75

Kindly let me know is there any settings I need to check or is it known behavior?

For your reference, I am attaching the logs.


rtc_timeout (tid:5)

Wakeup source is 0x82
>>> Start DA16X Supplicant ...
>>> TIM STATUS: 0x00000010
>>> TIM : FAST
DPM Mode = 1
[APP_SERIAL_COMM_COMMANDROUTERTASK] InputStreamBuffer created
[APP_SERIAL_COMM_RESPONDERTASK] OutputStreamBuffer created

===========================================

[ AWS-IOT Doorlock ]

[ Ver. 21.06 , 202106171700 , eoh ]

============================================


Using internal cert key by app_aws_certi.h


AWS_IOT on Station Mode for "143"

sleepMode: 3, rtcTime: 0


===========================================

[ Set Sleep mode : 3 , RTC time : 0 ,useRTM : 1 ]

============================================


[New Thread("DM_T_aws_shadowdpm") Start for DPM APP]


=============================================

[dpmAppThreadCreate] DPM mode checked...
"DM_IR_aws_shadowdpm" got dpm data size (12)
"DM_ER_aws_shadowdpm" got dpm data size (308)
Wake up from DPM Sleep

=============================================

"aws_shadowdpm" already registered to port #1883 for DPM process

sendDPMAppMSGQ...


============================
Wake mode [0x82] , type [1]
Wake up .... RTC timer
============================

[dpmAPPManager] DM_NEED_INIT
DM_INIT


AWS IoT SDK Version 3.0.1-

[Make AWS-Thing-Name]

[Built-name] AWS Thing name : [143] (len=3)

[dpmAPPManager] DM_NEED_CONNECTION
DM_NEED_CONNECTION

Shadow Init
WARN: [iot_tls_init:210] DPM Mode = 1
Shadow Connect
saved aws broker IP = "35.163.143.95"
sock(#=0) connect return (rc=0)
DEBUG: [iot_tls_connect:266] TLS processing after socket setup
[app_tls_restore:215] restore tls session OK, state = 16
[app_tls_restore] not the mode of receiving packet
[app_tls_setup:698] tls restore OK, but not UC wakeup
[app_socket_connect_tls] not the mode of receiving packet...bypass
DEBUG: [iot_tls_connect:324] saving binded port num=1883
DEBUG: [_aws_iot_mqtt_internal_connect:565] TCP & TLS session restored: go to fast wake-up step
Shadow Connection(DPM) OK
bypass the duplicated subscribing to AWS server (retry:0, wakeup type:1)
autoreconnect_status 0
Subscribing... 0
finish connection (rc=0)
[dpmAPPManager] DM_RTC_WAKEUP
DM_WAKEUP_TIMER


Sleep mode 3

[dpmAPPManager] DM_CHECK_RECV before DPM sleep
DM_FINISH_DEVICE

[dpmAPPManager] RTC_READY_POWER_DOWN
[dpm_keepalive_timer_register] RTC interval (=1200 secs), mode (=0)

... " goto DPM SLEEP...>þ
Wakeup source is 0x82
>>> Start DA16X Supplicant ...
>>> TIM STATUS: 0x00000001
>>> TIM : UC
DPM Mode = 1
[APP_SERIAL_COMM_COMMANDROUTERTASK] InputStreamBuffer created
[APP_SERIAL_COMM_RESPONDERTASK] OutputStreamBuffer created

===========================================

[ AWS-IOT Doorlock ]

[ Ver. 21.06 , 202106171700 , eoh ]

============================================


Using internal cert key by app_aws_certi.h


AWS_IOT on Station Mode for "143"

sleepMode: 3, rtcTime: 0


===========================================

[ Set Sleep mode : 3 , RTC time : 0 ,useRTM : 1 ]

============================================


[New Thread("DM_T_aws_shadowdpm") Start for DPM APP]


=============================================

[dpmAppThreadCreate] DPM mode checked...
"DM_IR_aws_shadowdpm" got dpm data size (12)
"DM_ER_aws_shadowdpm" got dpm data size (308)
Wake up from DPM Sleep

=============================================

"aws_shadowdpm" already registered to port #1883 for DPM process

sendDPMAppMSGQ...


============================
Wake mode [0x82] , type [2]
Wake up .... Recv Packet
============================

[dpmAPPManager] DM_NEED_INIT
DM_INIT


AWS IoT SDK Version 3.0.1-

[Make AWS-Thing-Name]

[Built-name] AWS Thing name : [143] (len=3)

[dpmAPPManager] DM_NEED_CONNECTION
DM_NEED_CONNECTION

Shadow Init
WARN: [iot_tls_init:210] DPM Mode = 1
Shadow Connect
saved aws broker IP = "35.163.143.95"
sock(#=0) connect return (rc=0)
DEBUG: [iot_tls_connect:266] TLS processing after socket setup
[app_tls_restore:215] restore tls session OK, state = 16
wake up read first . . .
Fail to read data: NETWORK_DISCONNECTED_ERROR (rc=-13)
DPM wake-up NETWORK_DISCONNECTED_ERROR
[app_tls_deinit:519] close (rc=0)
ERROR: [_aws_iot_mqtt_internal_connect:541] connect failed (socket or tls): re turn error: rc = -13
[aws_dpm_set_aws_server_ip:351] passed ip (="") invalid, and cleared
[app_tls_disconnect:1219] saved server's ip cleared
DEBUG: [iot_tls_destroy:437] IN
DEBUG: [iot_tls_destroy:439] OUT
ERROR: [AWS_DPM_App_Connect:2075] Shadow Connection Error (-13)
ERROR: [AWS_DPM_App_Connect:2314] Shadow Network Disconnected Error. go to ret ry connection: (rc=-13)
forced to disconnected
Free done
[AWS_DPM_App_Connect] reconnecting... (cnt=1)
Shadow Init
WARN: [iot_tls_init:210] DPM Mode = 1
Shadow Connect
aws broker URL = "a3lm5b0snjygjx-ats.iot.us-west-2.amazonaws.com"
new aws broker IP = "54.201.54.85"
sock(#=0) connect return (rc=0)
TLS setup needed
DEBUG: [iot_tls_connect:266] TLS processing after socket setup
setup tls connection newly
DEBUG: [iot_tls_connect:324] saving binded port num=1883
DEBUG: [_aws_iot_mqtt_internal_connect:594] aws mqtt connect OK
DEBUG: [_aws_iot_mqtt_internal_connect:618] send the connect packet : OK
DEBUG: [_aws_iot_mqtt_internal_connect:639] wait for the CONNACK: OK
Shadow Connection(DPM) OK
autoreconnect_status 0
Subscribing... 0
finish connection (rc=0)
[dpmAPPManager] DM_RECV_WAKEUP
DM_WAKEUP_RECV

DEBUG: [aws_dpm_wakeup_ready:174] DPM read len=0

force to sleep

Sleep mode 3

[dpmAPPManager] DM_CHECK_RECV before DPM sleep
DM_FINISH_DEVICE

[dpmAPPManager] RTC_READY_POWER_DOWN
[dpm_keepalive_timer_register] RTC interval (=1200 secs), mode (=0)

... " goto DPM SLEEP...>à

Regards,

Dipanjan

Parents Reply Children