Hi there,
I'm using DA16200MOD with AWS SDK version: DA16200_DA16600_SDK_v3.2.4.0_AWS_0 integrated in DA16200_DA16600_SDK_FreeRTOS_v3.2.4.0.
I have observed that when DA16200MOD is in sleep (SLEEP mode 3) with DPM settings (as below), device automatically wake-up after (approx. 20 mins).
DDPS Enable -NO
DPM Keep Alive Time- (Default 30000 ms)
DPM User Wakeup Time(0~86400 Sec.)- (Default 0 Sec.)
DPM TIM Wakeup Count(1~65535 dtim) - 75
Kindly let me know is there any settings I need to check or is it known behavior?
For your reference, I am attaching the logs.
rtc_timeout (tid:5)
Wakeup source is 0x82>>> Start DA16X Supplicant ...>>> TIM STATUS: 0x00000010>>> TIM : FASTDPM Mode = 1[APP_SERIAL_COMM_COMMANDROUTERTASK] InputStreamBuffer created[APP_SERIAL_COMM_RESPONDERTASK] OutputStreamBuffer created
===========================================
[ AWS-IOT Doorlock ]
[ Ver. 21.06 , 202106171700 , eoh ]
============================================
Using internal cert key by app_aws_certi.h
AWS_IOT on Station Mode for "143"
sleepMode: 3, rtcTime: 0
[ Set Sleep mode : 3 , RTC time : 0 ,useRTM : 1 ]
[New Thread("DM_T_aws_shadowdpm") Start for DPM APP]
=============================================
[dpmAppThreadCreate] DPM mode checked..."DM_IR_aws_shadowdpm" got dpm data size (12)"DM_ER_aws_shadowdpm" got dpm data size (308)Wake up from DPM Sleep
"aws_shadowdpm" already registered to port #1883 for DPM process
sendDPMAppMSGQ...
============================Wake mode [0x82] , type [1]Wake up .... RTC timer============================
[dpmAPPManager] DM_NEED_INITDM_INIT
AWS IoT SDK Version 3.0.1-
[Make AWS-Thing-Name]
[Built-name] AWS Thing name : [143] (len=3)
[dpmAPPManager] DM_NEED_CONNECTIONDM_NEED_CONNECTION
Shadow InitWARN: [iot_tls_init:210] DPM Mode = 1Shadow Connectsaved aws broker IP = "35.163.143.95"sock(#=0) connect return (rc=0)DEBUG: [iot_tls_connect:266] TLS processing after socket setup[app_tls_restore:215] restore tls session OK, state = 16[app_tls_restore] not the mode of receiving packet[app_tls_setup:698] tls restore OK, but not UC wakeup[app_socket_connect_tls] not the mode of receiving packet...bypassDEBUG: [iot_tls_connect:324] saving binded port num=1883DEBUG: [_aws_iot_mqtt_internal_connect:565] TCP & TLS session restored: go to fast wake-up stepShadow Connection(DPM) OKbypass the duplicated subscribing to AWS server (retry:0, wakeup type:1)autoreconnect_status 0Subscribing... 0finish connection (rc=0)[dpmAPPManager] DM_RTC_WAKEUPDM_WAKEUP_TIMER
Sleep mode 3
[dpmAPPManager] DM_CHECK_RECV before DPM sleepDM_FINISH_DEVICE
[dpmAPPManager] RTC_READY_POWER_DOWN[dpm_keepalive_timer_register] RTC interval (=1200 secs), mode (=0)
... " goto DPM SLEEP...>þWakeup source is 0x82>>> Start DA16X Supplicant ...>>> TIM STATUS: 0x00000001>>> TIM : UCDPM Mode = 1[APP_SERIAL_COMM_COMMANDROUTERTASK] InputStreamBuffer created[APP_SERIAL_COMM_RESPONDERTASK] OutputStreamBuffer created
============================Wake mode [0x82] , type [2]Wake up .... Recv Packet============================
Shadow InitWARN: [iot_tls_init:210] DPM Mode = 1Shadow Connectsaved aws broker IP = "35.163.143.95"sock(#=0) connect return (rc=0)DEBUG: [iot_tls_connect:266] TLS processing after socket setup[app_tls_restore:215] restore tls session OK, state = 16wake up read first . . .Fail to read data: NETWORK_DISCONNECTED_ERROR (rc=-13)DPM wake-up NETWORK_DISCONNECTED_ERROR[app_tls_deinit:519] close (rc=0)ERROR: [_aws_iot_mqtt_internal_connect:541] connect failed (socket or tls): re turn error: rc = -13[aws_dpm_set_aws_server_ip:351] passed ip (="") invalid, and cleared[app_tls_disconnect:1219] saved server's ip clearedDEBUG: [iot_tls_destroy:437] INDEBUG: [iot_tls_destroy:439] OUTERROR: [AWS_DPM_App_Connect:2075] Shadow Connection Error (-13)ERROR: [AWS_DPM_App_Connect:2314] Shadow Network Disconnected Error. go to ret ry connection: (rc=-13)forced to disconnectedFree done[AWS_DPM_App_Connect] reconnecting... (cnt=1)Shadow InitWARN: [iot_tls_init:210] DPM Mode = 1Shadow Connectaws broker URL = "a3lm5b0snjygjx-ats.iot.us-west-2.amazonaws.com"new aws broker IP = "54.201.54.85"sock(#=0) connect return (rc=0)TLS setup neededDEBUG: [iot_tls_connect:266] TLS processing after socket setupsetup tls connection newlyDEBUG: [iot_tls_connect:324] saving binded port num=1883DEBUG: [_aws_iot_mqtt_internal_connect:594] aws mqtt connect OKDEBUG: [_aws_iot_mqtt_internal_connect:618] send the connect packet : OKDEBUG: [_aws_iot_mqtt_internal_connect:639] wait for the CONNACK: OKShadow Connection(DPM) OKautoreconnect_status 0Subscribing... 0finish connection (rc=0)[dpmAPPManager] DM_RECV_WAKEUPDM_WAKEUP_RECV
DEBUG: [aws_dpm_wakeup_ready:174] DPM read len=0
force to sleep
... " goto DPM SLEEP...>à
Regards,
Dipanjan
Hi Dipanjan,Thank you for posting your question online. Let me check on this and I will get back to you.Kind Regards,OV_Renesas
Hi,
I would like to let you know that I have found out that below these two MACROS:
Hi Dipanjan,Thank you for the reply.I have raised an internal ticket so our team can check your logs and share why are you facing this wake-up issue. I will get back to you as soon as possible.Kind Regards,OV_Renesas