AT command to erase STA credentials

Hi,

I was trying to find an AT command to simply erase credentials stored by WFJAP command. I want to do that without doing a factory reset (ATF) or rebooting the da16200.

We are running base AT command set from Getting Started example on SDK 3.2.4.0.

Thanks,

Konstantin

Parents
  • Hi Konstantin,

    Even though there is no command to erase the STA credentials without rebooting or factory reset, you could use the AT+WFDIS command which is for making the Wi-Fi STA profile unused. After that, if you invoke AT+WFJAP with another STA credential then the profile will be updated.

    Please let me know if you have any questions.

    Kind Regards,
    OV_Renesas

Reply
  • Hi Konstantin,

    Even though there is no command to erase the STA credentials without rebooting or factory reset, you could use the AT+WFDIS command which is for making the Wi-Fi STA profile unused. After that, if you invoke AT+WFJAP with another STA credential then the profile will be updated.

    Please let me know if you have any questions.

    Kind Regards,
    OV_Renesas

Children
No Data