DA16200 SDK version

Hi,

In one of our projects, we're using the Sparkfun DA16200 WiFi shield. 
The user manual for the module advises updating the module with the most recent SDK version 
because it ships with an older SDK (SDK version 3.2.2.1). 
We are planning to use the HTTP, MQTT etc.  protocols in our final application. 
Is it safe to use the module with the SDK that comes pre-installed (3.2.2.1)? 
Or is the most recent version required to be updated?

Updating the module with latest sdk will be an overhead in our end product.

Parents Reply Children
No Data