DA16200 SDK 3.2.6 unable to build

I've installed the FreeRTOS SDK tool chain package (v1.0) and Eclipse version 2022-12 (4.26.0) on a clean/new Win10 laptop but I'm faced with a build error.:- 

10:59:06 **** Incremental Build of configuration Debug for project da16200 ****
make all
make: unknown option -- no-print-directory
BusyBox v1.36.0.git (2023-01-29 16:36:13 UTC)

Usage: make [--posix] [-C DIR] [-f FILE] [j NUM] [-eiknpqrsSt] [MACRO[::]=VAL]... [TARGET]...

Maintain files based on their dependencies

--posix Enforce POSIX mode
-C DIR Change to DIR
-f FILE Makefile
-j NUM Jobs to run in parallel (not implemented)
-e Environment variables override macros in makefiles
-i Ignore exit status
-k Continue on error
-n Dry run
-p Print macros and targets
-q Query target; exit status 1 if not up to date
-r Don't use built-in rules
-s Make silently
-S Stop on error
-t Touch files instead of making them
make: *** [makefile:121: all] Error 1
"make all" terminated with exit code 2. Build might be incomplete.

10:59:11 Build Failed. 1 errors, 0 warnings. (took 5s.101ms)

I've not found a solution on the web. Can you help?

I notice that during the install the text advised be that the install would require 3GB of HDD space! That's a lot of bloat!

I have another laptop - Win11 with Arm tools already installed but that also fails - in more interesting ways.- builds the DA16200.elf file but then fails with unable to find the file specified. I can grab logs and post here if I'm unable to get this machine building - I'm hoping to be able to find which tool it's looking for from a working buiild.

Thanks.

Keith_CQ.

Parents
  • Hello! 
    I am facing the exact same issue on a Win 11 machine without tools previously installed. 
    I followed the guide and ended up getting this same error:
    ```

    13:33:12 **** Build of configuration Debug for project da16600 ****
    make all
    make: unknown option -- no-print-directory
    BusyBox v1.36.0.git (2023-01-29 16:36:13 UTC)

    Usage: make [--posix] [-C DIR] [-f FILE] [j NUM] [-eiknpqrsSt] [MACRO[::]=VAL]... [TARGET]...

    Maintain files based on their dependencies

    --posix Enforce POSIX mode
    -C DIR Change to DIR
    -f FILE Makefile
    -j NUM Jobs to run in parallel (not implemented)
    -e Environment variables override macros in makefiles
    -i Ignore exit status
    -k Continue on error
    -n Dry run
    -p Print macros and targets
    -q Query target; exit status 1 if not up to date
    -r Don't use built-in rules
    -s Make silently
    -S Stop on error
    -t Touch files instead of making them
    make: *** [makefile:129: all] Error 1
    "make all" terminated with exit code 2. Build might be incomplete.

    13:33:14 Build Failed. 1 errors, 0 warnings. (took 1s.889ms)
    ```
    I am using this sdk: `DA16200_DA16600_SDK_FreeRTOS_v3.2.6.0`
    I have also extracted to a path with less than 70 chars length. 
    Please let us know for a solution. I am working on this about 2 weeks now.
    Thanks in advance 

  • Hi All,

    Our Team was able to recreate this issue.

    We found a compatibility issue with the compile environment.

    We are working on it to solve the issue.
    I will update you here as soon as I have an update from the Team that the issue is fixed.

    Kind Regards,
    OV_Renesas

  • I am just getting started with the EVK, and I am experiencing the same build issue. I also look forward to the solution.

  • Update: I found that the SDK builds with Eclipse 2021-03 but breaks with Eclipse 2021-06. So for anyone needing to play with the SDK before the fix is released, try the older version of Eclipse.

  • Hi, Michael

    Thanks for your infomation.

    I tried builds SDK version v3.2.6 with 2021-03.

    but, Unfortunatery I was facing the Making Error....

    xxxx/xpacks/@xpack-dev-tools/arm-none-eabi-gcc/10.2.1-1.1.2/.content/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld.exe: 
    cannot find -lramlib
    cannot find -lumac
    cannot find -lwpa_cli
    cannot find -lsupplicant
    cannot find -llmac
    cannot find -ldpm
    cannot find -lcryptolib
    cannot find -lcryptopkg
    cannot find -lromac

     Eclips Info:

    Eclipse 
    Version: 2021-03 (4.19.0)
    Build id: 20210312-0638

    I look forward to the Renesas Team's solution.

    Best regarts.

  • In case it makes any difference, I am running on Windows 10.

Reply Children