DA16200 Abnormal DPM and timer wake ups

Hello,

my application needs periodic wake ups at the exact time. I have set up a periodic timer through the DPM manager config callback. The problem is that while there is no wi-fi connection(Abnoraml DPM) the timer stops working. There are no wake-ups by the timer anymore. Is there any solution to make it run even in the Abnormal DPM mode?

rtc_timeout (tid:5)
 [timer1_callback] Called by timer1...
!!! No selected network !!!

rtc_timeout (tid:5)
 [timer1_callback] Called by timer1...
!!! No selected network !!!
>> Abnormal DPM(1) operation after 1 second.

Wakeup source is 0x82


System Mode : Station Only (0)
>>> Start DA16X Supplicant ...
>>> DA16x Supp Ver2.7 - 2022_03
>>> Wi-Fi mode : b/g/n -> b/g (for DPM)
>>> MAC address (sta0) : d4:3d:39:10:ec:6a
>>> sta0 interface add OK
>>> Start STA mode...
 [tcp_server_dpm_sample] Start TCP Server Sample
 [tcp_server_dpm_sample_load_server_info] TCP Server Information(10190)
 [tcp_server_dpm_sample_init_callback] Boot initialization
>>> Hello World #1 ( Non network dependent application ) !!!
!!! No selected network !!!

rtc_timeout (tid:5)
 [timer1_callback] Called by timer1...
!!! No selected network !!!
…

  • Hi HanKo,

    Thank you for posting your question online and for your interest in our Wi-Fi products.
    Yes, you can configure the DPM Manager to wake you up in abnormal sleep mode as well.
    You can set the sleep time in abnormal DPM by configuring the _user_defined_wakeup_interval.
    You must make sure you have defined the __USER_DPM_ABNORM_WU_INTERVAL__ macro on the config_generic_sdk.h file:

    //-----------------------
    // DPM Features
    //-----------------------
    
        //
        // Enable/Disable DPM Abnormal wakeup User-timer
        //  This values are used to define DPM abnormal wakeup interval time.
        //
        //  Default values are defined in ~/library/libdpm.a
        //   : const unsigned long long dpm_monitor_retry_interval[DPM_MON_RETRY_CNT] = {
        //         ULLONG_MAX,    // Initial value : ULLONG_MAX
        //         60,            // 1st Wakeup
        //         60,            // 2nd Wakeup    : 0xdeadbeaf for no-wakeup
        //         60,            // 3rd Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 4th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 5th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 6th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 60,       // 7th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 60,       // 8th Wakeup    : 0xdeadbeaf for no-wakeup
        //         0xDEADBEAF     // 9th Wakeup    : 0xdeadbeaf for no-wakeup
        //     };
        //
        //  When enable this feature,
        //   user can set these values to any value they want
        //   in ~/apps/da16200/get_started/src/user_main/system_start.c :
        //
        //   : unsigned long long _user_defined_wakeup_interval[DPM_MON_RETRY_CNT] = {
        //         ULLONG_MAX,    // Initial value : ULLONG_MAX
        //         60,            // 1st Wakeup
        //         60,            // 2nd Wakeup    : 0xdeadbeaf for no-wakeup
        //         60,            // 3rd Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 4th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 5th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 30,       // 6th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 60,       // 7th Wakeup    : 0xdeadbeaf for no-wakeup
        //         60 * 60,       // 8th Wakeup    : 0xdeadbeaf for no-wakeup
        //         0xDEADBEAF     // 9th Wakeup    : 0xdeadbeaf for no-wakeup
        //     };
        #define __USER_DPM_ABNORM_WU_INTERVAL__

    Then you can find the appropriate function to configure this variable on the system_start.c file:
    /*
     * Format of dpm abnormal wakeup interval
     *
     *  value allowed for wakeup interval
     *                 1 : mininum
     *          0x1FFFFF : maximum, 24 days
     *        0xDEADBEAF : no wakeup
     *       wrong value : < 1 or > 0x1FFFFF, set to 3600 sec (default)
     *
     *  Example:
     *     unsigned long long _user_defined_wakeup_interval[];
     *     {
     *         ULLONG_MAX,            // Initial value : ULLONG_MAX
     *         10, 10, 10, 10, 10,
     *         60,
     *         3600,
     *         3600,
     *         3600 * 24
     *     }
     */
    unsigned long long _user_defined_wakeup_interval[DPM_MON_RETRY_CNT] = {
        ULLONG_MAX,            // Initial value : ULLONG_MAX
        60,                    // 1st Wakeup
        60,                    // 2nd Wakeup    : 0xdeadbeaf for no-wakeup
        60,                    // 3rd Wakeup    : 0xdeadbeaf for no-wakeup
        60 * 30,               // 4th Wakeup    : 0xdeadbeaf for no-wakeup
        60 * 30,               // 5th Wakeup    : 0xdeadbeaf for no-wakeup
        60 * 30,               // 6th Wakeup    : 0xdeadbeaf for no-wakeup
        60 * 60,               // 7th Wakeup    : 0xdeadbeaf for no-wakeup
        60 * 60,               // 8th Wakeup    : 0xdeadbeaf for no-wakeup
        0xDEADBEAF             // 9th Wakeup    : 0xdeadbeaf for no-wakeup
    };
    
    static void set_dpm_abnorm_user_wakeup_interval(void)
    {
    #if defined ( __USER_DPM_ABNORM_WU_INTERVAL__ )
        dpm_abnorm_user_wakeup_interval = (unsigned long long *)_user_defined_wakeup_interval;
    #endif // __USER_DPM_ABNORM_WU_INTERVAL__
    }

    Which SDK version are you using?

    Kind Regards,
    OV_Renesas