DA16200 put "Hard Fault Exception" with AT+NWHTC.

Hi,
I use US159-DA16200MEVZ with AT Command.
When I tried acceess to AWS s3 use on AT+NWHTC(with presigned URL), DA16200 put "Hard Fault Exception".
Presigned URL is long(over 1500 character) URL Data.

AT Command

AT+NWHTC=https://xxxxxxxx....xxxxxxx,get

Debug Message

And, I confirmed same issue with dummy long URL.
AT Command

AT+NWHTC=https://aaaaaaa...aaaaaaa,get

Debug Message

When I used dummy short long URL, Hard Fault is not occured.

AT Command

AT+NWHTC=https://aaaaa,get

OK

+NWHTCSTATUS:3

Debug Message

Read CA(length = 0)
Read Cert(length = 0)
Read Privkey(length = 0)

[httpc_cb_result_fn:674]httpc_result: 3, received: 0 byte, err: -16

so, I think maybe over DA16200's URL limit size.
I want to solve this problem.
I would greatly appreciate any feedback, guidance, or suggestions that the Renesas community can provide.

My SDK Information is...

Wakeup source is 0x4
[dpm_init_retmemory] DPM INIT CONFIGURATION(1)


        ******************************************************
        *             DA16200 SDK Information
        * ---------------------------------------------------
        *
        * - CPU Type        : Cortex-M4 (120MHz)
        * - OS Type         : FreeRTOS 10.4.3
        * - Serial Flash    : 4 MB
        * - SDK Version     : V3.2.3.0 GEN-ATCMD
        * - F/W Version     : FRTOS-GEN01-01-56c232799-004158
        * - F/W Build Time  : Jun  3 2022 16:56:46
        * - Boot Index      : 0
        *
        ******************************************************



System Mode : Station Only (0)

Best Regarts.

  • Hi There,

    Thank you for posting your question online.
    From the logs you have shared I can see that you are using a quite old SDK version (v3.2.3). Is there a reason you are not using the latest SDK version?
    We highly recommend to use the latest SDK version v3.2.6 which you can find here:https://www.renesas.com/eu/en/document/sws/da16200-da16600-freertos-sdk-v3260?r=1600096
    You can find the pre-compiled images here: https://www.renesas.com/eu/en/document/sws/da16200-da16600-freertos-sdk-image-v3260?r=1600096
    Regarding the issue you are facing with AT+NWHTC:
    The maximum url string length is 256 bytes. That is why you were facing a Hard Fault Exception.

    You should search on the user_http_client.h file and change:

    #define HTTPC_MAX_PATH_LEN			256

    and change it to:
    #define HTTPC_MAX_PATH_LEN            (1024 * 2)

    This way you can query at least 2kB URL string length.
    The Max request data can be set through the below definiotins in the same file:
    // Max size of HTTP Client's request data
    #define HTTPC_MAX_REQ_DATA            (1024 * 4)

    Note: Keep in mind that Max request data cannot be over the stack size:
    // Stack size of HTTP Client
    #define    HTTPC_STACK_SZ                (1024 * 6) // Max 10KB

    If the HTTP buffer is increased, AT command buffer size should also be increased inside the atcmd.h file:
    #define    TX_PAYLOAD_MAX_SIZE        (1024 * 8) // Max 8KB


    Kind Regards,
    OV_Renesas
  • Hi OV_Renesas,

    Thanks for your answer.

    I want to try this suggestions but now I'm facing bellow same problem and I can not build SDK version v3.2.6 on windows.

    https://community.renesas.com/wireles-connectivity/f/wi-fi/29990/da16200-sdk-3-2-6-unable-to-build

    for now, I wait this issue is solved.

    Best Regarts.

  • Hi There,

    Thank you for the reply.
    I will update you here as well when this issue is fixed.

    Kind Regards,
    OV_Renesas

  • Hi OV_Renesas,

    Thanks for your support.

    The build now works for me on Windows 11 ver.21H2 and Eclipse 2023-03 (4.27.0) 

    And I tried to up url string length, so, Hard Fault with url string length is gone.

    #define HTTPC_MAX_PATH_LEN            (1024 * 2)

    Thanks a lot!!

    and... now I'm facing bellow new 2 issue. 

    1. ERROR -682 Occured.

    When I send AT+NWHTC Continuously, somtimes AT+NWHTC respond ERROR -682.

    (maybe this error -> AT_CMD_ERR_NW_HTC_TASK_CREATE_FAIL              = -682,)

    When this error is responded, do I retry command until "OK HTTP/1.1 200 OK"?

    Or, Do I wait any STATUS?

    e.g.

    AT+NWHTC=https://xxxxx,put,Message1
    OK HTTP/1.1 200 OK
    
    AT+NWHTC=https://xxxxx,put,Message2
    ERROR:-682
    +NWHTCSTATUS:0
    
    AT+NWHTC=https://xxxxx,put,Message3
    OK HTTP/1.1 200 OK

    2. Hard Fault Exception

    Maybe, related to the "1. ERROR -682 Occured"

    When I send bellow AT+NWHTC, DA16200 put "Hard Fault Exception".

    Is there a way to avoid Hard Fault?

    AT+NWHTC=https://xxxxxx,put,Message1
    OK HTTP/1.1 200 OK
    
    AT+NWHTC=https://xxxxxx,get
    ERROR:-682
    +NWHTCSTATUS:0
    
    AT+NWHTC=https://xxxxxx,get
    OK HTTP/1.1 200 OK
    
    [Hard Fault]
    +NWHTCSTATUS:0
    +INIT:DONE,0
    

    Debug Message

    I confirmed this issue too with bellow version.

    DA16200_IMG_FreeRTOS_ATCMD_QFN_v3.2.6.0_4MB

    I would greatly appreciate any feedback, guidance, or suggestions that the Renesas community can provide.

    Best Regarts.

  • Hi There,

    Thank you for the reply.
    Glad you were able to build SDK v3.2.6 and for being able to get rid off the Hard Fault error for the URL string.
    Regarding the new 2 errors you are facing, let me check on this and I will get back to you as soon as possible.

    Kind Regards,
    OV_Renesas

  • Hi There,

    Apologies for the delay.
    Regarding the Error: -682
    The root cause of this error was that MCU sent the AT+NWHTC command before it had received the +NWHTCSTATUS:0 response.

    The normal sequence is like below:
    1. MCU will send "AT+NWHTC=">">https://xxxxx,put,Message1" command.
    2. MCU will receive "OK" response.(Then, the MCU can send another command (for instance: AT+VER) except "AT+NWHTC" to DA16200. You cannot send again the AT+NWHTC command because it is still working)
    3.Finally, if the MCU receives "+NWHTCSTATUS:0" response, then the MCU can send next AT+NWHTC command.

    Please test after changing the sequence on the MCU side.
    Regarding the Hard Fault Error:
    We were not able to reproduce this error after trying multiple times. 
    Can you please clarify if you faced the error -682 and the hard fault error with the official (pre-compiled) binary (DA16200_IMG_FreeRTOS_ATCMD_QFN_v3.2.6.0_4MB) or if it happened with your own custom binary? If it happened with your own custom binary, could you please provide a map file so we can investigate it?
    Can you also kindly share how many times (how often) are you able to reproduce the hard fault error?
    Finally, could you please test again after changing the sequence of the MCU? (MCU send the next AT+NWHTC command only after it has received the +NWHTCSTATUS response)

    Best Regards,
    OV_Renesas

  • Hi OV_Renesas,

    Thanks your answer!!

    I will try your suggestions "Changing the sequence of the MCU".

     

  • HI There,

    Thank you for the reply.
    Please share any feedback if you faced the Error: -682 and the Hard Fault error after changing the sequence of the MCU.

    Kind Regards,
    OV_Renesas

  • Sorry I mistake log file.
    I put again.

    Hi OV_Renesas,

    Thanks your support.

    I tried to change sequence (Wait +NWHTCSTATUS Response).

    so,
    Error: -682 was gone. Thanks a lot!!!

    But... I faced Hard Fault too.
    I insert log (with masked private information)

    - DEBUG LOG

    Wakeup source is 0x4 
    [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    
    
    	******************************************************
    	*             DA16200 SDK Information
    	* --------------------------------------------------- 
    	*
    	* - CPU Type        : Cortex-M4 (120MHz)
    	* - OS Type         : FreeRTOS 10.4.3
    	* - Serial Flash    : 4 MB
    	* - SDK Version     : V3.2.6.0 GEN-ATCMD
    	* - F/W Version     : FRTOS-GEN01-01-df31adb8a-006190
    	* - F/W Build Time  : Feb  9 2023 13:58:04
    	* - Boot Index      : 0
    	*
    	******************************************************
    
    
    
    System Mode : Station Only (0)
    >>> Start DA16X Supplicant ...
    >>> DA16x Supp Ver2.7 - 2022_03
    >>> MAC address (sta0) : XXXXXXXXXXXXXXXXXXXXXXXXXX
    >>> sta0 interface add OK
    >>> Start STA mode...
    
    >>> UART1 : Clock=80000000, BaudRate=115200
    >>> UART1 : DMA Enabled ...
    
    >>> Network Interface (wlan0) : UP
    >>> Associated with XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    Connection COMPLETE to XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    -- DHCP Client WLAN0: SEL(6)
    -- DHCP Client WLAN0: REQ(1)
    
    ### User Call-back : Success to connect Wi-Fi ...
    -- DHCP Client WLAN0: CHK(8)
    -- DHCP Client WLAN0: BOUND(10)
    	 Assigned addr   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       netmask   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       gateway   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       DNS addr  : XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    	 DHCP Server IP  : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	 Lease Time      : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	 Renewal Time    : XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    
    all Delete success.
    Read CA(length = 1469)
    Read Cert(length = 0)
    Read Privkey(length = 0)
    HTTP-Client request to https://XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    hdr_len : 318, content_len : 0
    
    httpc_result: 0, received: 0 byte, err: 0
    Read CA(length = 1469)
    Read Cert(length = 0)
    Read Privkey(length = 0)
    HTTP-Client request to https://XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    hdr_len : 422, content_len : 14
    
    httpc_result: 0, received: 14 b
     Fault_count:1 Fault_PC:0x8ba62 
    
     [Hard Fault Exception]
    
    Register-Dump
    	R0  :20086746,	R1  :00000100,	R2  :000adaa8,	R3  :000ada88
    	R4  :00000001,	R5  :000992fd,	R6  :a5a5a5a5,	R7  :a5a5a5a5
    	R8  :a5a5a5a5,	R9  :a5a5a5a5,	R10 :a5a5a5a5,	R11 :a5a5a5a5
    	R12 :a5a5a5a5,	SP  :00080ddc,	LR  :0008ba55,	PC  :0008ba62
    	PSR :2100000e,	EXC :fffffff1,
    Fault Status
    	SHCSR :00000400,	CFSR  :01000000,	HFSR  :40000000
    	DFSR  :00000000,	MMFAR :e000ed34,	BFAR  :e000ed38
    	AFSR  :00000000,
    SysInfo
    	SICS[0] = 04300000
    	SICS[1] = 00000000
    	SICS[2] = 00000000
    	SICS[3] = 00000000
    	SICS[4] = 00000000
    	SICS[5] = 015f4571
    
    Stack-Dump (48)
    [0x00080ddc] : 00000001 00F00000 00000007 C0000018 00093654 0015C2F9 0015C198 41000000 
    [0x00080dfc] : 5B594B7D 4F4F5053 01405A3F ECE96B58 797DFD7C 20086746 00000100 000ADAA8 
    [0x00080e1c] : 000ADA88 00000001 000992FD A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 A5A5A5A5 
    [0x00080e3c] : A5A5A5A5 A5A5A5A5 00080DDC 0008BA55 0008BA62 2100000E FFFFFFF1 A5A5A5A5 
    [0x00080e5c] : 00000001 00F00000 00000007 C0000018 00093654 0015C2F9 0015C198 41000000 
    [0x00080e7c] : 5B594B7D 4F4F5053 01405A3F ECE96B58 797DFD7C 20086746 00000100 000ADAA8 
    
    Current Thread
    	 Thread: 
    	 stack ptr : 20086746
    	 stack base: 68004808
    	 stack end : 81f0e8bd
    	 stack high: 20086746
    	 max usage : 61e88178
    	 suspend   : 00000159
    
    Thread Stack (0)
    
    
    Wakeup source is 0x1 
    [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    
    
    	******************************************************
    	*             DA16200 SDK Information
    	* --------------------------------------------------- 
    	*
    	* - CPU Type        : Cortex-M4 (120MHz)
    	* - OS Type         : FreeRTOS 10.4.3
    	* - Serial Flash    : 4 MB
    	* - SDK Version     : V3.2.6.0 GEN-ATCMD
    	* - F/W Version     : FRTOS-GEN01-01-df31adb8a-006190
    	* - F/W Build Time  : Feb  9 2023 13:58:04
    	* - Boot Index      : 0
    	*
    	******************************************************
    
    
    
    ....
    
    

    -AT COMMNAD LOG (with Time Stamp)

    [2023-03-31T10:45:08.762382]
    AT+NWMQCL=0
    
    [2023-03-31T10:45:10.766886]
    OK
    
    [2023-03-31T10:45:10.766886]
    AT+NWDCRT
    
    [2023-03-31T10:45:12.769099]
    OK
    
    [2023-03-31T10:45:12.769099]
    C3,
    [2023-03-31T10:45:12.882107]
    -----BEGIN CERTIFICATE-----
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    -----END CERTIFICATE-----
    
    [2023-03-31T10:45:14.893011]
    OK
    
    [2023-03-31T10:45:14.893011]
    AT+NWCCRT
    
    [2023-03-31T10:45:16.897208]
    +NWCCRT:32
    OK
    
    [2023-03-31T10:45:16.902978]
    AT+NWHTC=https://XXXXXXXXXXXXXXXXXXXXXXXXXX,put,Hello World !!
    
    [2023-03-31T10:45:18.906398]
    OK
    HTTP/1.1 200 OK
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Date: Fri, 31 Mar 2023 01:45:14 GMT
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Server: XXXXXXXXXXXXXXXXXXXXXXXXXX
    Content-Length: 0
    Connection: close
    
    
    [2023-03-31T10:45:20.908293]
    +NWHTCSTATUS:0
    
    [2023-03-31T10:45:20.909552]
    AT+NWHTC=https://XXXXXXXXXXXXXXXXXXXXXXXXXX,get
    
    [2023-03-31T10:45:22.916644]
    OK
    HTTP/1.1 200 OK
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Date: Fri, 31 Mar 2023 01:45:18 GMT
    Last-Modified: Fri, 31 Mar 2023 01:45:14 GMT
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Accept-Ranges: bytes
    Content-Type: binary/octet-stream
    Server: XXXXXXXXXXXXXXXXXXXXXXXXXX
    Content-Length: 14
    Connection: close
    
    Hello World !!
    [2023-03-31T10:45:24.918005]
    +NWHTCSTATUS:0
    
    +INIT:DONE,0
    
    ....
    
    +WFJAP:1,XXXXXXXXXXXXXXXXXXXXXXXXXX,XXXXXXXXXXXXXXXXXXXXXXXXXX
    

    And I faced another pattern ASSERT vPortFree 405/406.
    This Pattern is not Hard Fault, but debug log put ASSERT vPortFree 405/406.
    I insert log too.
    - DEBUG LOG

    Wakeup source is 0x4 
    [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    
    
    	******************************************************
    	*             DA16200 SDK Information
    	* --------------------------------------------------- 
    	*
    	* - CPU Type        : Cortex-M4 (120MHz)
    	* - OS Type         : FreeRTOS 10.4.3
    	* - Serial Flash    : 4 MB
    	* - SDK Version     : V3.2.6.0 GEN-ATCMD
    	* - F/W Version     : FRTOS-GEN01-01-df31adb8a-006190
    	* - F/W Build Time  : Feb  9 2023 13:58:04
    	* - Boot Index      : 0
    	*
    	******************************************************
    
    
    
    System Mode : Station Only (0)
    >>> Start DA16X Supplicant ...
    >>> DA16x Supp Ver2.7 - 2022_03
    >>> MAC address (sta0) : XXXXXXXXXXXXXXXXXXXXXXXXXX
    >>> sta0 interface add OK
    >>> Start STA mode...
    
    >>> UART1 : Clock=80000000, BaudRate=115200
    >>> UART1 : DMA Enabled ...
    
    >>> Network Interface (wlan0) : UP
    >>> Associated with XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    Connection COMPLETE to XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    -- DHCP Client WLAN0: SEL(6)
    -- DHCP Client WLAN0: REQ(1)
    
    ### User Call-back : Success to connect Wi-Fi ...
    -- DHCP Client WLAN0: CHK(8)
    -- DHCP Client WLAN0: BOUND(10)
    	 Assigned addr   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       netmask   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       gateway   : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	       DNS addr  : XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    	 DHCP Server IP  : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	 Lease Time      : XXXXXXXXXXXXXXXXXXXXXXXXXX
    	 Renewal Time    : XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    
    all Delete success.
    Read CA(length = 1469)
    Read Cert(length = 0)
    Read Privkey(length = 0)
    HTTP-Client request to https://XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    hdr_len : 350, content_len : 0
    
    httpc_result: 0, received: 0 byte, err: 0
    Read CA(length = 1469)
    Read Cert(length = 0)
    Read Privkey(length = 0)
    HTTP-Client request to https://XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    hdr_len : 318, content_len : 0
    
    httpc_result: 0, received: 0 byte, err: 0
    Read CA(length = 1469)
    Read Cert(length = 0)
    Read Privkey(length = 0)
    HTTP-Client request to https://XXXXXXXXXXXXXXXXXXXXXXXXXX
    
    hdr_len : 422, content_len : 14
    
    httpc_result: 0, received: 14 b>> ASSERT vPortFree 405 !!! 
    >> ASSERT vPortFree 406 !!! 
    yte, err: 0
    

    -AT COMMNAD LOG (with Time Stamp)

    [2023-03-31T11:02:26.741221]
    AT+NWMQCL=0
    
    [2023-03-31T11:02:28.748969]
    OK
    
    [2023-03-31T11:02:28.748969]
    AT+NWDCRT
    
    [2023-03-31T11:02:30.754103]
    OK
    
    [2023-03-31T11:02:30.756124]
    C3,
    [2023-03-31T11:02:30.865919]
    -----BEGIN CERTIFICATE-----
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    -----END CERTIFICATE-----
    
    [2023-03-31T11:02:32.881220]
    OK
    
    [2023-03-31T11:02:32.883737]
    AT+NWCCRT
    
    [2023-03-31T11:02:34.886191]
    +NWCCRT:32
    OK
    
    [2023-03-31T11:02:34.886191]
    AT+NWHTC=https://XXXXXXXXXXXXXXXXXXXXXXXXXX,put,Hello World !!
    
    [2023-03-31T11:02:36.901782]
    OK
    HTTP/1.1 200 OK
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Date: Fri, 31 Mar 2023 02:02:33 GMT
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Server: XXXXXXXXXXXXXXXXXXXXXXXXXX
    Content-Length: 0
    Connection: close
    
    
    [2023-03-31T11:02:38.905763]
    +NWHTCSTATUS:0
    
    [2023-03-31T11:02:38.907780]
    AT+NWHTC=https://XXXXXXXXXXXXXXXXXXXXXXXXXX,put,Hello World !!
    
    [2023-03-31T11:02:40.916666]
    OK
    HTTP/1.1 200 OK
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Date: Fri, 31 Mar 2023 02:02:36 GMT
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Server: XXXXXXXXXXXXXXXXXXXXXXXXXX
    Content-Length: 0
    Connection: close
    
    
    [2023-03-31T11:02:42.920276]
    +NWHTCSTATUS:0
    
    [2023-03-31T11:02:42.920276]
    AT+NWHTC=https://XXXXXXXXXXXXXXXXXXXXXXXXXX,get
    
    [2023-03-31T11:02:44.932326]
    OK
    HTTP/1.1 200 OK
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Date: Fri, 31 Mar 2023 02:02:40 GMT
    Last-Modified: Fri, 31 Mar 2023 02:02:36 GMT
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    XXXXXXXXXXXXXXXXXXXXXXXXXX
    Accept-Ranges: bytes
    Content-Type: binary/octet-stream
    Server: XXXXXXXXXXXXXXXXXXXXXXXXXX
    Content-Length: 14
    Connection: close
    
    Hello World !!
    [2023-03-31T11:02:46.936357]
    +NWHTCSTATUS:0
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    

    I would greatly appreciate any feedback/suggestions.


    Finally, I will answer the following.

    > official (pre-compiled) binary (DA16200_IMG_FreeRTOS_ATCMD_QFN_v3.2.6.0_4MB) or if it happened with your own custom binary?

    I use official (pre-compiled) binary (DA16200_IMG_FreeRTOS_ATCMD_QFN_v3.2.6.0_4MB).
    And I changed MQTT TLS buffer size on debug window refer to the bellow.

    Da16200 connecting to AWS

    [/DA16200/NVRAM] # nvram
     Command-List is changed, "NVRAM"
    [/DA16200/NVRAM] # setenv MQTT_TLS_INCOMING 16384
    [/DA16200/NVRAM] #
    [/DA16200/NVRAM] # setenv MQTT_TLS_OUTGOING 16384
    [/DA16200/NVRAM] # reboot

    > how many times (how often) are you able to reproduce the hard fault error?

    When I send Https PUT -> Https GET, Hard Fault or ASSERT vPortFree one or the other always occurs.

    Best Regarts.