Introduction:
We have a custom board that uses a RA6M4 MCU to control a DA16600 over a UART using the AT commands. The device is working fine and I can use AT commands to make connections to our AWS implementation. I was test driving different DA16600 builds to explore the DA16600 AWS implementation. Now I want to go back to just the standard DA16600 AT command image, but I can't identify which image to use.
The images that are available that work with my hardware implementation seem to also implement a demo application. I'm about to dig into enabling DPM power management and want to make sure the image I'm using is not doing anything I don't expect it to.
My Question:
Is there a DA16600 image that does not implement any demo code that I can use?
---------------------------------------------------------------------------------------------------------------------------------------------
Details on how I tried to find an image:
New DA16600 Image (FreeRTOS v3.2.8.0):
I went to the DA16600MOD page, and downloaded the DA16200 DA16600 FreeRTOS SDK Image v3.2.8.0.
Inside this zip file there are 7 additional zip files:
I attempted to load and verify each of the images contained in the download hopping to find the correct image . . .
DA16200_IMG_FreeRTOS_ATCMD_SPI_EVK_v3.2.8.0_4MB
DA16200_IMG_FreeRTOS_ATCMD_SPI_SPARKFUN_v3.2.8.0_4MB
DA16200_IMG_FreeRTOS_QFN_v3.2.8.0_4MB
DA16600_IMG_FreeRTOS_ATCMD_SPI_EVK_v3.2.8.0_4MB
DA16600_IMG_FreeRTOS_ATCMD_UART2_EVK_v3.2.8.0_4MB
******************************************************
* DA16600 SDK Information
* ---------------------------------------------------
*
* - CPU Type : Cortex-M4 (120MHz)
* - OS Type : FreeRTOS 10.4.3
* - Serial Flash : 4 MB
* - SDK Version : V3.2.8.0 GEN-ATCMD
* - F/W Version : FRTOS-GEN01-01-f017bfdf51-006558
* - F/W Build Time : Aug 10 2023 14:09:33
* - Boot Index : 0
Start of UDP Socket sample, gas leak event(0)
iot_sensor connected to server
DA16600_IMG_FreeRTOS_QFN_v3.2.8.0_4MB
* - SDK Version : V3.2.8.0 GEN
* - F/W Build Time : Aug 10 2023 13:55:45
>>> Hello World #2 ( network dependent application ) !!!
Just as a reference I captured the DA16600 firmware image that shipped on the DA16600 from a second device.
* - SDK Version : V3.2.5.0 GEN-ATCMD
* - F/W Version : FRTOS-GEN01-01-1f66deb8b-006084
* - F/W Build Time : Feb 28 2023 17:57:29
[combo][iot_sensor]
is_provisioned = 1
is_sensor_started = 0
Hi Brian,Thank you for posting your question online.
BrianW said:I was test driving different DA16600 builds to explore the DA16600 AWS implementation. Now I want to go back to just the standard DA16600…
Thank you for the details. I've successfully built, loaded and used the clean image!