Failed to publish to a topic in AWS

I'm using DA 16200mod evk  to publish to a topic in Aws. Downloaded the DA16200 firmware image '.ttl'  script from DA16200_DA16600_AWS_v3.2.8.0_ATCMD_img. Have sent the three certificates files over uart.I have done the configurations using AT commands sending from nRF52840 DK uart, as follows

"AT+AWS=SET APP_THINGNAME tap-pet-nrf-device\r\n");
   
("AT+AWS=SET AWS_BROKER a3kbzziaf9hg4n-ats.iot.us-east-1.amazonaws.com\r\n");
    ("AT+AWS=SET APP_LPORT 8443\r\n");
    ("AT+AWS=CFG 0 sample/pet 0 0\r\n");
    ("AT+AWS=CMD MCU_DATA 0 sample/pet 25\n\r");
All in station mode
As per the manual after this a factory reset is to be done which leads to soft ap mode and waiting for provisioning. But here it is entering soft AP mode but no wfscan happens or provisioning cannot be done. 
In teraterm I'm getting it with error as shown below (when nrf transmits AT COMMANDS to DA)
  • Hi,

    As a follow up, I tired with the downloaded precompiled image to see whether I will be able to connect to any networks through the app.  I could reach till the wifi provisioning this time, but again the connection to the AWS server did not happen and then the DA went to sleep mode 2.  I had a hard time bringing to out from the sleep mode since I was not using an MCU at this point.  

    Later I wanted to give you a log file with the wifi provisioning attempts included. 

    [2023-12-01 14:05:41.824] 
    [2023-12-01 14:05:41.824] argv[0]:ATZ
    [2023-12-01 14:05:41.824] 
    [2023-12-01 14:05:41.824] Usage: ATZ=
    [2023-12-01 14:05:45.200] 
    [2023-12-01 14:05:45.200] argv[0]:ATE
    [2023-12-01 14:05:45.200] 
    [2023-12-01 14:05:45.200] Usage: ATE=[<?>]
    [2023-12-01 14:05:57.810] 
    [2023-12-01 14:05:57.810] argv[0]:AT+WFMODE
    [2023-12-01 14:05:57.810] argv[1]:0
    [2023-12-01 14:05:57.810] 
    [2023-12-01 14:05:57.810] Usage: AT+WFMODE=<mode>
    [2023-12-01 14:06:07.678] 
    [2023-12-01 14:06:07.678] argv[0]:AT+WFJAPA
    [2023-12-01 14:06:07.678] argv[1]:Linksys07692
    [2023-12-01 14:06:07.678] argv[2]:aryamaryjose
    [2023-12-01 14:06:07.678] 
    [2023-12-01 14:06:07.678] Usage: AT+WFJAPA=<ssid>[,<key>][,<hidden>]
    [2023-12-01 14:06:18.720] 
    [2023-12-01 14:06:18.720] argv[0]:AT+WFJAPA
    [2023-12-01 14:06:18.720] argv[1]:Linksys07692
    [2023-12-01 14:06:18.720] argv[2]:aryamaryjose
    [2023-12-01 14:06:18.720] 
    [2023-12-01 14:06:18.720] Usage: AT+WFJAPA=<ssid>[,<key>][,<hidden>]
    [2023-12-01 14:06:21.610] 
    [2023-12-01 14:06:21.610] Wakeup source is 0x4 
    [2023-12-01 14:06:21.610] [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    [2023-12-01 14:06:21.625] 
    [2023-12-01 14:06:21.625] 
    [2023-12-01 14:06:21.625] 	******************************************************
    [2023-12-01 14:06:21.625] 	*             DA16200 SDK Information
    [2023-12-01 14:06:21.625] 	* --------------------------------------------------- 
    [2023-12-01 14:06:21.625] 	*
    [2023-12-01 14:06:21.625] 	* - CPU Type        : Cortex-M4 (120MHz)
    [2023-12-01 14:06:21.625] 	* - OS Type         : FreeRTOS 10.4.3
    [2023-12-01 14:06:21.625] 	* - Serial Flash    : 4 MB
    [2023-12-01 14:06:21.625] 	* - SDK Version     : V3.2.8.0 AWS-ATCMD Doorlock Ref. QFN GEN
    [2023-12-01 14:06:21.625] 	* - F/W Version     : FRTOS-GEN01-01-f017bfdf51-006558
    [2023-12-01 14:06:21.645] 	* - F/W Build Time  : Nov 30 2023 13:23:08
    [2023-12-01 14:06:21.645] 	* - Boot Index      : 0
    [2023-12-01 14:06:21.645] 	*
    [2023-12-01 14:06:21.645] 	******************************************************
    [2023-12-01 14:06:21.645] 
    [2023-12-01 14:06:21.645] 
    [2023-12-01 14:06:21.645]  Not define feature and set Default EVK
    [2023-12-01 14:06:21.645] 
    [2023-12-01 14:06:21.645]  EVK Doorlock or Default EVK (current board=0)
    [2023-12-01 14:06:21.645] 
    [2023-12-01 14:06:21.673] 
    [2023-12-01 14:06:21.673] System Mode : Station Only (0)
    [2023-12-01 14:06:21.673] >>> Start DA16X Supplicant ...
    [2023-12-01 14:06:21.688] >>> DA16x Supp Ver2.7 - 2022_03
    [2023-12-01 14:06:21.688] >>> MAC address (sta0) : d4:3d:39:38:e7:da
    [2023-12-01 14:06:21.688] >>> sta0 interface add OK
    [2023-12-01 14:06:21.688] >>> Start STA mode...
    [2023-12-01 14:06:21.821] [atcmd_transport_set_max_session:9479]Set max session(8), max CID(9)
    [2023-12-01 14:06:21.821] [atcmd_network_get_sess_info:10540]Load sess_info(len:1240, cnt:10)
    [2023-12-01 14:06:21.821] 
    [2023-12-01 14:06:21.821] >>> UART1 : Clock=80000000, BaudRate=115200
    [2023-12-01 14:06:21.821] >>> UART1 : DMA Enabled ...
    [2023-12-01 14:06:21.821] 
    [2023-12-01 14:06:21.833] Start AT Command 
    [2023-12-01 14:06:21.833] [UART ready notification]
    [2023-12-01 14:06:21.833] [atcmd_network_delete_sess_info:10594]Start
    [2023-12-01 14:06:22.633] RTC switched to XTAL
    [2023-12-01 14:06:25.993] 
    [2023-12-01 14:06:25.993] Wakeup source is 0x4 
    [2023-12-01 14:06:26.011] [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    [2023-12-01 14:06:26.011] 
    [2023-12-01 14:06:26.011] 
    [2023-12-01 14:06:26.011] 	******************************************************
    [2023-12-01 14:06:26.011] 	*             DA16200 SDK Information
    [2023-12-01 14:06:26.011] 	* --------------------------------------------------- 
    [2023-12-01 14:06:26.011] 	*
    [2023-12-01 14:06:26.011] 	* - CPU Type        : Cortex-M4 (120MHz)
    [2023-12-01 14:06:26.011] 	* - OS Type         : FreeRTOS 10.4.3
    [2023-12-01 14:06:26.011] 	* - Serial Flash    : 4 MB
    [2023-12-01 14:06:26.011] 	* - SDK Version     : V3.2.8.0 AWS-ATCMD Doorlock Ref. QFN GEN
    [2023-12-01 14:06:26.030] 	* - F/W Version     : FRTOS-GEN01-01-f017bfdf51-006558
    [2023-12-01 14:06:26.030] 	* - F/W Build Time  : Nov 30 2023 13:23:08
    [2023-12-01 14:06:26.030] 	* - Boot Index      : 0
    [2023-12-01 14:06:26.030] 	*
    [2023-12-01 14:06:26.030] 	******************************************************
    [2023-12-01 14:06:26.030] 
    [2023-12-01 14:06:26.030] 
    [2023-12-01 14:06:26.030]  Not define feature and set Default EVK
    [2023-12-01 14:06:26.030] 
    [2023-12-01 14:06:26.030]  EVK Doorlock or Default EVK (current board=0)
    [2023-12-01 14:06:26.030] 
    [2023-12-01 14:06:26.056] 
    [2023-12-01 14:06:26.056] System Mode : Station Only (0)
    [2023-12-01 14:06:26.056] >>> Start DA16X Supplicant ...
    [2023-12-01 14:06:26.072] >>> DA16x Supp Ver2.7 - 2022_03
    [2023-12-01 14:06:26.072] >>> MAC address (sta0) : d4:3d:39:38:e7:da
    [2023-12-01 14:06:26.072] >>> sta0 interface add OK
    [2023-12-01 14:06:26.072] >>> Start STA mode...
    [2023-12-01 14:06:26.137] [atcmd_transport_set_max_session:9479]Set max session(8), max CID(9)
    [2023-12-01 14:06:26.137] [atcmd_network_get_sess_info:10540]Load sess_info(len:1240, cnt:10)
    [2023-12-01 14:06:26.137] 
    [2023-12-01 14:06:26.137] >>> UART1 : Clock=80000000, BaudRate=115200
    [2023-12-01 14:06:26.152] >>> UART1 : DMA Enabled ...
    [2023-12-01 14:06:26.152] 
    [2023-12-01 14:06:26.152] Start AT Command 
    [2023-12-01 14:06:26.152] [UART ready notification]
    [2023-12-01 14:06:26.152] [atcmd_network_delete_sess_info:10594]Start
    [2023-12-01 14:06:27.002] RTC switched to XTAL
    [2023-12-01 14:06:31.928] 
    [2023-12-01 14:06:31.928] argv[0]:ATZ
    [2023-12-01 14:06:31.928] 
    [2023-12-01 14:06:31.928] Usage: ATZ=
    [2023-12-01 14:06:34.168] 
    [2023-12-01 14:06:34.168] argv[0]:ATE
    [2023-12-01 14:06:34.168] 
    [2023-12-01 14:06:34.168] Usage: ATE=[<?>]
    [2023-12-01 14:06:43.945] 
    [2023-12-01 14:06:43.945] argv[0]:AT+WFMODE
    [2023-12-01 14:06:43.945] argv[1]:0
    [2023-12-01 14:06:43.945] 
    [2023-12-01 14:06:43.945] Usage: AT+WFMODE=<mode>
    [2023-12-01 14:07:03.243] 
    [2023-12-01 14:07:03.243] argv[0]:AT+WFJAPA
    [2023-12-01 14:07:03.243] argv[1]:Linksys07692
    [2023-12-01 14:07:03.243] argv[2]:aryamaryjose
    [2023-12-01 14:07:03.243] FAIL
    [2023-12-01 14:07:03.243] 0
    [2023-12-01 14:07:03.243] 
    [2023-12-01 14:07:04.043] 
    [2023-12-01 14:07:04.043] >>> Network Interface (wlan0) : UP
    [2023-12-01 14:07:04.043] >>> Associated with e8:9f:80:35:84:aa
    [2023-12-01 14:07:04.154] 
    [2023-12-01 14:07:04.154] Connection COMPLETE to e8:9f:80:35:84:aa
    [2023-12-01 14:07:04.154] 
    [2023-12-01 14:07:04.154] -- DHCP Client WLAN0: SEL(6)
    [2023-12-01 14:07:04.170] 
    [2023-12-01 14:07:04.170] ### User Call-back : Success to connect Wi-Fi ...
    [2023-12-01 14:07:05.562] -- DHCP Client WLAN0: REQ(1)
    [2023-12-01 14:07:05.562] -- DHCP Client WLAN0: CHK(8)
    [2023-12-01 14:07:06.077] -- DHCP Client WLAN0: BOUND(10)
    [2023-12-01 14:07:06.077] 	 Assigned addr   : 192.168.11.146
    [2023-12-01 14:07:06.077] 	       netmask   : 255.255.255.0
    [2023-12-01 14:07:06.077] 	       gateway   : 192.168.11.1
    [2023-12-01 14:07:06.077] 	       DNS addr  : 192.168.11.1
    [2023-12-01 14:07:06.077] 
    [2023-12-01 14:07:06.077] 	 DHCP Server IP  : 192.168.11.1
    [2023-12-01 14:07:06.077] 	 Lease Time      : 24h 00m 00s
    [2023-12-01 14:07:06.077] 	 Renewal Time    : 12h 00m 00s
    [2023-12-01 14:07:06.077] 
    [2023-12-01 14:07:06.077] 
    [2023-12-01 14:07:06.077] Usage: AT+WFJAPA=<ssid>[,<key>][,<hidden>]
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] ===========================================
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] [ APP-IOT AT-COMMAND ] 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] [ aws_shadow_dpm_auto_start]
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] AWS_IOT on Station Mode for "test_aws_iot" 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] ============================================
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] [pal_app_dpm_auto_start] mcu_wakeup_port=-1, mcu_wakeup_pin=0x0 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] default set to mcu_wakeup_port=0, mcu_wakeup_pin=0x800 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] 
    [2023-12-01 14:07:06.096] Root CA: O
    [2023-12-01 14:07:06.096] Certificate: O
    [2023-12-01 14:07:06.104] Private Key: O
    [2023-12-01 14:07:06.104] 
    [2023-12-01 14:07:06.104] nvram read string(broker) error
    [2023-12-01 14:07:06.104] 
    [2023-12-01 14:07:06.104] invalid APP feature...can't start APP Platform thread...check again
    [2023-12-01 14:07:06.104] 
    [2023-12-01 14:07:06.104] 
    [2023-12-01 14:07:06.104] >>latestStatus : 5
    [2023-12-01 14:07:32.345] 
    [2023-12-01 14:07:32.345] ======================================================= 
    [2023-12-01 14:07:32.345] argc num = 2 
    [2023-12-01 14:07:32.345] argv[0]: AT+AWS
    [2023-12-01 14:07:32.345] argv[1]: SET APP_THINGNAME vani_aws_iot
    [2023-12-01 14:07:32.345] =======================================================
    [2023-12-01 14:07:32.345] APP SET vani_aws_iot 
    [2023-12-01 14:07:43.690] 
    [2023-12-01 14:07:43.690] ======================================================= 
    [2023-12-01 14:07:43.705] argc num = 2 
    [2023-12-01 14:07:43.705] argv[0]: AT+AWS
    [2023-12-01 14:07:43.705] argv[1]: SET APP_PUBTOPIC vani_aws_iot/DeviceControl
    [2023-12-01 14:07:43.705] =======================================================
    [2023-12-01 14:07:43.705] APP SET vani_aws_iot/DeviceControl 
    [2023-12-01 14:07:54.186] 
    [2023-12-01 14:07:54.186] ======================================================= 
    [2023-12-01 14:07:54.202] argc num = 2 
    [2023-12-01 14:07:54.202] argv[0]: AT+AWS
    [2023-12-01 14:07:54.202] argv[1]: SET AWS_BROKER a3kbzziaf9hg4n-ats.iot.us-east-1.amazonaws.com
    [2023-12-01 14:07:54.202] =======================================================
    [2023-12-01 14:07:54.202] APP SET a3kbzziaf9hg4n-ats.iot.us-east-1.amazonaws.com 
    [2023-12-01 14:08:22.538] 
    [2023-12-01 14:08:22.538] ======================================================= 
    [2023-12-01 14:08:22.538] argc num = 2 
    [2023-12-01 14:08:22.538] argv[0]: AT+AWS
    [2023-12-01 14:08:22.538] argv[1]: CFG 1 mcu_door 1 0
    [2023-12-01 14:08:22.538] =======================================================
    [2023-12-01 14:08:22.538] 
    [2023-12-01 14:08:22.538] =======================================================
    [2023-12-01 14:08:22.538] Att[1] number   : 1
    [2023-12-01 14:08:22.538] Att[1] name     : mcu_door
    [2023-12-01 14:08:22.538] Att[1] data type: 1
    [2023-12-01 14:08:22.553] Att[1] MQTT type: 0
    [2023-12-01 14:08:22.554] =======================================================
    [2023-12-01 14:08:22.554] 
    [2023-12-01 14:10:09.370] 
    [2023-12-01 14:10:09.370] [/DA16200] # net
    [2023-12-01 14:10:16.923]     Command-List is changed, "NET"
    [2023-12-01 14:10:16.923] [/DA16200/NET] # cert status
    [2023-12-01 14:10:21.099] 
    [2023-12-01 14:10:21.099] #1:
    [2023-12-01 14:10:21.099]   For MQTT, CoAPs Client
    [2023-12-01 14:10:21.099]   - Root CA     : Found
    [2023-12-01 14:10:21.099]   - Certificate : Found
    [2023-12-01 14:10:21.099]   - Private Key : Found
    [2023-12-01 14:10:21.099]   - DH Parameter: Empty
    [2023-12-01 14:10:21.115] 
    [2023-12-01 14:10:21.115] #2:
    [2023-12-01 14:10:21.115]   For HTTPs, OTA
    [2023-12-01 14:10:21.115]   - Root CA     : Empty
    [2023-12-01 14:10:21.115]   - Certificate : Empty
    [2023-12-01 14:10:21.115]   - Private Key : Empty
    [2023-12-01 14:10:21.115]   - DH Parameter: Empty
    [2023-12-01 14:10:21.115] 
    [2023-12-01 14:10:21.115] #3:
    [2023-12-01 14:10:21.115]   For Enterprise (802.1x)
    [2023-12-01 14:10:21.115]   - Root CA     : Empty
    [2023-12-01 14:10:21.115]   - Certificate : Empty
    [2023-12-01 14:10:21.130]   - Private Key : Empty
    [2023-12-01 14:10:21.130]   - DH Parameter: Empty
    [2023-12-01 14:10:21.130] 
    [2023-12-01 14:10:21.130] TLS_CERT for ATCMD
    [2023-12-01 14:10:21.130]   - TLS_CERT_01 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_02 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_03 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_04 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_05 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_06 : Empty
    [2023-12-01 14:10:21.130]   - TLS_CERT_07 : Empty
    [2023-12-01 14:10:21.147]   - TLS_CERT_08 : Empty
    [2023-12-01 14:10:21.147]   - TLS_CERT_09 : Empty
    [2023-12-01 14:10:21.147]   - TLS_CERT_10 : Empty
    [2023-12-01 14:10:21.147] 
    [2023-12-01 14:10:21.147] [/DA16200/NET] # top
    [2023-12-01 14:10:24.282]     Command-List is changed, "ROOT"
    [2023-12-01 14:10:24.282] [/DA16200] # 
    [2023-12-01 14:10:45.691] ======================================================= 
    [2023-12-01 14:10:45.691] argc num = 2 
    [2023-12-01 14:10:45.691] argv[0]: AT+AWS
    [2023-12-01 14:10:45.691] argv[1]: CMD RESET_TO_AP
    [2023-12-01 14:10:45.691] =======================================================
    [2023-12-01 14:10:45.706] 
    [2023-12-01 14:10:45.706] board feature : 
    [2023-12-01 14:10:45.706]  TO AP resetMode
    [2023-12-01 14:10:45.706] 
    [2023-12-01 14:10:45.706] DA16200 factory reset AP mode = 1 ("AP_ONLY")....
    [2023-12-01 14:10:45.785] .....[app_set_customer_ap_configure] set AP config mode = 1 
    [2023-12-01 14:10:45.834] 
    [2023-12-01 14:10:45.834] apps_reboot_ap_mode  Customer configuration ...
    [2023-12-01 14:10:45.834] .
    [2023-12-01 14:10:45.899]  default_ssid = "Dialog_DA16200" ..., ap_config_param->ssid_name 
    [2023-12-01 14:10:45.899] 
    [2023-12-01 14:10:45.899]  PW = 1234567890 
    [2023-12-01 14:10:45.899] 
    [2023-12-01 14:10:45.899]  PW = 1234567890  completed
    [2023-12-01 14:10:45.899] .
    [2023-12-01 14:10:45.899] apps_reboot_ap_mode  IPADDR_CUSTOMER...
    [2023-12-01 14:10:45.914] ....
    [2023-12-01 14:10:45.947] apps_reboot_ap_mode  customer_dhcpd_flag == DHCPD_CUSTOMER..
    [2023-12-01 14:10:45.947] ......
    [2023-12-01 14:10:46.058] OK
    [2023-12-01 14:10:46.058] 
    [2023-12-01 14:10:46.058] 
    [2023-12-01 14:10:46.461] 
    [2023-12-01 14:10:46.461] Wakeup source is 0x0 
    [2023-12-01 14:10:46.461] [dpm_init_retmemory] DPM INIT CONFIGURATION(1)
    [2023-12-01 14:10:46.461] 
    [2023-12-01 14:10:46.461] 
    [2023-12-01 14:10:46.461] 	******************************************************
    [2023-12-01 14:10:46.477] 	*             DA16200 SDK Information
    [2023-12-01 14:10:46.477] 	* --------------------------------------------------- 
    [2023-12-01 14:10:46.477] 	*
    [2023-12-01 14:10:46.477] 	* - CPU Type        : Cortex-M4 (120MHz)
    [2023-12-01 14:10:46.477] 	* - OS Type         : FreeRTOS 10.4.3
    [2023-12-01 14:10:46.477] 	* - Serial Flash    : 4 MB
    [2023-12-01 14:10:46.477] 	* - SDK Version     : V3.2.8.0 AWS-ATCMD Doorlock Ref. QFN GEN
    [2023-12-01 14:10:46.477] 	* - F/W Version     : FRTOS-GEN01-01-f017bfdf51-006558
    [2023-12-01 14:10:46.493] 	* - F/W Build Time  : Nov 30 2023 13:23:08
    [2023-12-01 14:10:46.493] 	* - Boot Index      : 0
    [2023-12-01 14:10:46.493] 	*
    [2023-12-01 14:10:46.493] 	******************************************************
    [2023-12-01 14:10:46.493] 
    [2023-12-01 14:10:46.493] 
    [2023-12-01 14:10:46.493]  Not define feature and set Default EVK
    [2023-12-01 14:10:46.493] 
    [2023-12-01 14:10:46.493]  EVK Doorlock or Default EVK (current board=0)
    [2023-12-01 14:10:46.493] 
    [2023-12-01 14:10:46.523] 
    [2023-12-01 14:10:46.523] System Mode : Soft-AP (1)
    [2023-12-01 14:10:46.523] 
    [2023-12-01 14:10:46.523] >>> DHCP Server Started
    [2023-12-01 14:10:46.523] >>> Start DA16X Supplicant ...
    [2023-12-01 14:10:46.571] >>> DA16x Supp Ver2.7 - 2022_03
    [2023-12-01 14:10:46.571] >>> Add SoftAP Inteface (softap1) ...
    [2023-12-01 14:10:46.571] >>> MAC address (softap1) : d4:3d:39:38:e7:db
    [2023-12-01 14:10:46.587] >>> softap1 interface add OK
    [2023-12-01 14:10:46.587] >>> AP Operating Channel: 1(2412)
    [2023-12-01 14:10:46.587] 
    [2023-12-01 14:10:46.587] >>> Network Interface (wlan1) : UP
    [2023-12-01 14:10:46.587] >>> BSS Isolate Disabled
    [2023-12-01 14:10:46.587] 
    [2023-12-01 14:10:46.587] Soft-AP is Ready (d4:3d:39:38:e7:db)
    [2023-12-01 14:10:46.634] [atcmd_transport_set_max_session:9479]Set max session(8), max CID(9)
    [2023-12-01 14:10:46.634] [atcmd_network_get_sess_info:10540]Load sess_info(len:1240, cnt:10)
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] >>> UART1 : Clock=80000000, BaudRate=115200
    [2023-12-01 14:10:46.652] >>> UART1 : DMA Enabled ...
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] Start AT Command 
    [2023-12-01 14:10:46.652] [UART ready notification]
    [2023-12-01 14:10:46.652] [atcmd_network_delete_sess_info:10594]Start
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] ===========================================
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] [ APP-IOT AT-COMMAND ] 
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] [ aws_shadow_dpm_auto_start]
    [2023-12-01 14:10:46.652] 
    [2023-12-01 14:10:46.652] ============================================
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] [pal_app_dpm_auto_start] mcu_wakeup_port=-1, mcu_wakeup_pin=0x0 
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] default set to mcu_wakeup_port=0, mcu_wakeup_pin=0x800 
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] Root CA: O
    [2023-12-01 14:10:46.669] Certificate: O
    [2023-12-01 14:10:46.669] Private Key: O
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] shadow item count = 0, (integer#=0, string#=0, float#=0)
    [2023-12-01 14:10:46.669] nvram read shadow config error
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] invalid APP feature...can't start APP Platform thread...check again
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] 
    [2023-12-01 14:10:46.669] >>latestStatus : 5
    [2023-12-01 14:11:18.395] AP-STA-CONNECTED 22:d2:bd:fb:84:4b
    [2023-12-01 14:11:18.395] 
    [2023-12-01 14:11:18.395] ### User Call-back : Success to connect Wi-Fi ...
    
     

    I have 3 questions at this point-

    1.  After the hard reset and provisioning, is it possible to wake up the DA from the DPM sleep mode in any simple way?   Since AT commands were not exactly possible in this mode, by giving any external pulses to the RT_WAKEup pin is it supposed to come out?  I had to use power switch and reset and finally a reloading of the image to get it working.

    2.  Why is it not listing any networks when I used our custom image, a hard reset and invoked provisioning as shown in this image?

    3.  Please go through the attached log and help me understand if any issues with AWS IOT setup.  The device shadow and certificates are attached to the thing as shown here.  

    I hope you will be able to give me a solution and get my DA working finally

    Thanks and Regards,

    Raji

  • Hi Raji,

    Thank you for the replies.
    Let me take a look on these and I will get back to you as soon as possible.
    I will try to do a detailed step by step on how to use the AWS with the Mobile application.

    Best Regards,
    OV_Renesas

  • Hi,

    Thank you for your kind reply.  I thought of also sharing the console o/p which I received on trying the initial hard reset.  Hope this along with the logs will help you to understand the DA not listing the available ssid's on using the built image.  Please note that I have not made any changes in the SDK file other than enabling the debug logs as instructed.

    Thanks and Regards,

    Raji

  • Hi Raji,

    Thank you for the reply and apologies for the delay.
    I wanted to let you know that we are still working on this.

    Best Regards,
    OV_Renesas

  • Hi,

    Any updates? I wanted to let you know that the AWS configuration is good since I could manage to publish via a different sdk once.  I tried provisioning via the setup command using teraterm.  Not using the provisioning app.  I tried downloading the sdk again from your server using this link- https://www.renesas.com/us/en/products/wireless-connectivity/wi-fi/low-power-wi-fi/da16200mod-ultra-low-power-wi-fi-modules-battery-powered-iot-devices?downloads-title-filter=image#design_development.  Its now back to MQTT bad parameters and packet id 0.  Could you please help me with this SDK issues since I'm really falling on time.

    Appreciate a speedy response.

    Thanks and Regards,

    raji

  • Hi, 

    With the sdk which helped me connect to MQTT and publish to AWS , the AT command window is not becoming active now.  Even on reset, the +init 0 is not getting displayed or commands cannot be typed (higher port, baud rate:115200).  Including a screenshot of the response i recieved on flashing the image - 

    Please provide me with an SDK which can connect to the AWS and in which MQTT connection is possible.  This is urgent.  Request your speedy response

    Regards,

    raji

  • Hi Raji,

    Thank you for the replies and apologies for the delay.
    We are sorry for any inconvenience our delay has created.
    Glad you were able to use the MQTT commands and publish to AWS.
    Regarding the AT command window:
    On UART0 during boot-up, you should see the following (highlighted) lines, that would show that the UART2 has been initialized for AT commands:

    If you are not able to see those lines, it means that you have not enabled the AT commands on the generic SDK.

    In order to do that, please go on config_generic_sdk.h file:

    You will have to define the __SUPPORT_ATCMD__.
    If the __SUPPORT_MQTT__ macro is defined (which is defined by default), the MQTT client feature would be enabled on the image created by the building process.
    This is documented on the UM-WI-003, on section 4.1.1 How to Run AT-CMD on UART, on page: 26

    Best Regards,
    OV_Renesas

  • Hi Raji,

    I forgot to mention the following:
    On the same file (config_generic_sdk.h file) please make sure you have defined the __SUPPORT_MQTT__ macro on the line 850. You will need to do this only if you define the __SUPPORT_AWS_IOT__ macro as well

    	// AWS IoT Platform define from project config
    #if defined ( __SUPPORT_AWS_IOT__ ) || defined ( __SUPPORT_AZURE_IOT__ )
    	#undef __SUPPORT_DPM_MANAGER__				// use or not DPM manager
    	
        #if defined ( __SUPPORT_WIFI_CONCURRENT__ )
            #undef __SUPPORT_WIFI_CONCURRENT__
            #define __SUPPORT_FACTORY_RST_APMODE__              // Factory reset AP-Mode
            #undef  __SUPPORT_FACTORY_RST_STAMODE__             // Factory reset STA-Mode
        #endif
    
    	#if !defined ( __SUPPORT_FACTORY_RESET_BTN__ )
    		#define	__SUPPORT_FACTORY_RESET_BTN__
    	#endif
    
    	#if defined ( __SUPPORT_WPS_BTN__ )
    		#undef	__SUPPORT_WPS_BTN__				// WPS button
    	#endif
    
    	#if !defined ( __SET_WAKEUP_HW_RESOURCE__ )
    		#define __SET_WAKEUP_HW_RESOURCE__		// RTC_WAKEUP_PIN1/2
    	#endif
    
    	#if defined ( __SUPPORT_WIFI_PROVISIONING__ )
    		#undef  __SUPPORT_WIFI_PROVISIONING__		// AP Provisioning operation with Phone APP
    	#endif
    
    	#if defined ( __SUPPORT_HELLO_WORLD__ )
    		#undef	__SUPPORT_HELLO_WORLD__
    	#endif
    
    	#if defined ( __SUPPORT_MQTT__ )
    		#undef	__SUPPORT_MQTT__				// Support MQTT
    	#endif
    
    	#if defined ( __SUPPORT_IPERF__ )
    		#undef	__SUPPORT_IPERF__				// IPerf
    	#endif
    	
    	#if !defined ( __SUPPORT_OTA__ )
    		#define __SUPPORT_OTA__
    	#endif
    
    	#if defined ( __SUPPORT_WEBSOCKET_CLIENT__ )
    		#undef	__SUPPORT_WEBSOCKET_CLIENT__	// websocket client
    	#endif
    
    #endif // __SUPPORT_AWS_IOT__
    


    Best Regards,
    OV_Renesas

  • Hi OV_Renesas,

    Thank you for your reply.  __SUPPORT_ATCMD__.and  __SUPPORT_MQTT__  are defined in the file. uart1 and 2 messages are also present.   But there is also an error which is status 5, ( ATCMD_Status_need_configuration = 5).  How do I correct this in the file.  Also could the MQTT publish error be due to this?  Why exactly is the pBuffer is Null error is coming when trying t publish?

    Regards,

    raji

  • Hi Raji,

    Happy New Year!
    Apologies for all the delay but the Renesas Engineering Team was OOO the last 2 weeks.

    But there is also an error which is status 5, ( ATCMD_Status_need_configuration = 5).  How do I correct this in the file.

    Is this an error when you are trying to compile the project or while trying to run the project?

      Also could the MQTT publish error be due to this?

    Yes, that would be possible. If the Macros where not properly defined on the images you used, you would not be able to use the MQTT publish feature.

    Why exactly is the pBuffer is Null error is coming when trying t publish?

    This could be related with a Heap exhaustion issue. How much data are you trying to publish at one time? 
    On the FreeRTOSConfig.h file, you can increase the Heap. And you should handle the memory allocation on every task you have created on your project.

    #ifdef INTEGRATION_WITH_RTOS_HEAP
    #define configTOTAL_HEAP_SIZE					( ( size_t ) ( 300 * 1024 ) )
    #else
    #define configTOTAL_HEAP_SIZE					( ( size_t ) ( 200 * 1024 ) )
    #endif
    


    Best Regards,
    OV_Renesas