Encountering Problems Loading Image on DA16600 Custom Board

Hello everyone,

I'm currently working on a project involving a custom board based on the DA16600 chip, and I've encountered an issue while trying to load an image onto it. I've attached a screenshot below for reference.

Additionally, I've included the circuit diagram of my custom board to provide more context.

The problem arises when I attempt to load the image onto the board. Despite following the usual procedures, I'm facing difficulties in getting it to work properly. I've double-checked the connections and configurations, but the issue persists.

I would greatly appreciate any insights or suggestions on what might be causing this problem and how I can resolve it. Has anyone else encountered similar challenges with the DA16600 chip or similar custom boards? Any advice or guidance would be immensely helpful.

Thank you in advance for your assistance!

Parents Reply
  • Hi There,

    Thank you for the reply.
    I am not aware if you are a colleague of Trainyinfy, which created this thread. So I am a bit confused on your issue. 
    You have the exact same schematic as shared in the original post? 
    You have applied the WatchDog Patch on SDK v3.2.8.1, compiled and downloaded which project? 
    Please create a new thread with all the information gathered there. Schematic, SDK version, UART0 logs, etc.

    Best Regards,
    OV_Renesas

Children