Hi,
I'm completely new to the DA16600 - is there any documentation on the images contained in the 'DA16200_DA16600_IMG_FreeRTOS_v3.2.8.1' download? The '_ATCMD_' images I can guess, but what is 'DA16600_IMG_FreeRTOS_QFN_v3.2.8.1_4MB'? The readme file gives no clue.
Thanks,
Hi There,Thank you for posting your question online.The pre-compiled images provided contain the Getting Started example of the FreeRTOS SDK v3.2.8.1. The _ATCMD_ images contain the Getting Started Example with the AT commands feature enabled.Since you are new with the DA16600MOD please refer on the following Guides/Tutorial:UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide (renesas.com)UM-WI-046 DA16200 DA16600 FreeRTOS SDK Programmer Guide (renesas.com)UM-WI-003 DA16200 DA16600 Host Interface and AT Command User Manual (renesas.com)UM-WI-030 DA16200 DA16600 DPM User Manual (renesas.com)Best Regards,OV_Renesas
Thanks - I've been reading the documents you suggest (and have installed the SDK in e2 studio) but I'm hoping to avoid getting into the details of the SDK and simply wish to use all the device features with AT commands; are all the AT commands supported in the image files? My question is similar to the one below in that I just want to use the device with AT commands and not have to customise the image.
community.renesas.com/.../which-da16600-image-should-i-use-for-the-basic-freertos-uart-at-cmd-build
Hi There,Thank you for the reply.You can use the already pre-compiled image for AT commands.All the AT commands listed on UM-WI-003 are supported by the AT-CMD image.Best Regards,OV_Renesas