Apostrophe in SSID name results in erroneous WFJAP=? response

When trying to connect to SSID with a non-utf8 apostrophe (in our case, it's the "right single quote" U+2019: https://www.compart.com/en/unicode/U+2019), DA16K successfully connects to the AP but then when querying WFJAP, responds with erroneous SSID (in this case 0617061e2809973207769666 as opposed to papa's wifi). See attached log screenshot.

Chip: DA16200

SDK: RTOS 3.2.8.5

 

Parents Reply
  • The apostrophe should be in the SSID, not the password. The windows may not allow it, but some routers do. I was able to set up my router with a right apostrophe in the SSID name.

    Try with a different router if you can't do it in windows because we have customers that have right apostrophes in their SSID name and I was able to set it up on my router as well.

    This is definitely an issue for us.

Children