Hello Team,
i got this module today,i just want to know this module come with build in SDK or we have to load in this after we got if not come with SDK then which SDK file we have to load. i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using UART0 as you suggest me UART0 is for debug and UART1 is for AT command) .....but after waiting some time i end the task.because it not loading..
what is the correct way to load the file and which one is correct. because i am using with HOST controller.i have RX71 controller and i want to communicate via using AT command i want to send data on IOT page using AT command and i am MQTT
protocol. Thanks and regard's AK
Hi AK,Thank you for posting your question online.
ak said: i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using
Were you able to see the progress bar on Tera Term? If there is no progress during the download please stop the procedure and try again.
ak said: what is the correct way to load the file and which one is correct.
Please refer on the UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide (renesas.com), on section 5.7 Programming Firmware Images in e2studio. and on section 5.7.3 Programming Firmware Images Using SEGGER J-LinkYou can also find pre-compiled binaries on the DA16200 Product site: DA16200 - Ultra-Low Power Wi-Fi SoC for Battery-Powered IoT Devices | Renesas
Best Regards,OV_Renesas
Hello OV Renesas, Thanks for replay, i am not using EVB DA16600 EVB Hardware Configuration. I am just using DA16200 module with rx71 microcontroller UART without EVB board can we send pre-compiled binaries images in the module.
Here i am not giving VBAT only using RX TX GND connection like RX-TX and TX-RX and GND from FTDI module to DA16200. and also tried with VBAT supply given.
here i am using UART0 is using for loading this TTL file.(i tried for UART1 also as the second image you will see that side UART1 connection is there but as you told this is for AT Command) but for both UART0 and UART1 the file issue get same.
in this image of tera term after this ttl file loading second step that i did is send the image file using YMOD but it sending the bar is not increasing.
i am using FTDI module CP2102 does this will affect for this issue because they are using FT232 IC and you have
using DSD TECH SH-U09C5 and this have IC FT232RL.or i have to take different FTDI module
and i also install drivers for the FTDI and also set the baudrate 230400.
i read on PDF there are saying that reset button should be pressed while loading the file which PIN should i connect the switch of DA16200module i attched the PDF screenshot.
or i am controlled from MCU so i connect PWR RTC KEY to VBAT as your PDF have information.
thanks and regard
AK.
Hello, at first SDK is load but next time i doing but it's not loading.is there have only one time loading provision have this module or any thing different step to load this SDK.thanks and regard's
hello,
for the first time SDK load into module and then i check AT command ATZ to get OK command its not working
for this AT command have any CR,CR+LF transmitted text setting.
kindly give replay as soon as possible i am stuck in project.
thanks and regard's
AK
Hi AK,Thank you for the reply.
ak said: for the first time SDK load into module and then i check AT command ATZ to get OK command its not working for this AT command have any CR,CR+LF transmitted text setting.
Yes, when you sent the AT commands you should also change the line. This is achieved with CR+LF. If this does not work, please probe a logic analyzer on the UART lines and share the catpure with us.Best Regards,OV_Renesas
Hello, 1) As you suggest the send the AT command with CR+LF.i did the same and also check the UART1 PIN connected with my scope but in that there is no waveform not generate i have attached the pic.
2) I have read in one datasheet there is external clock source required but in the schematic there is no pin i seen is it for another or the same. 3) Does the RTC required external clock source. because when i powered the RTC_PWR_KEY with VBAT SDK is load but when i do it for next time SDK is not loading.is it because of RTC clock is not connected or is there any another reason.
i attached the PDF screenshot for this RTC clock issue kindly see any revert as soon as possible.
Best Regard's
Hello,
This is give me error CRC failed while loading.and i will check the AT command and this will not give me OK response.why this happen.
i did hardware connection the PDF application schematic show's
like this ckt design i did hardware connection I did RTC_wake_up2-GND, VDD_DIO2 and VDD_DIO1,VBAT,RTC wake up,rtc pwr key give 3.3V.
Hi AK,Thank you for the replies and apologies for the delay.
ak said: 1) As you suggest the send the AT command with CR+LF.i did the same and also check the UART1 PIN connected with my scope but in that there is no waveform not generate i have attached the pic.
Based on the Screenshot you shared from UART0 on your next reply, the FW is not running and it is then expected that the AT commands will not work.
ak said: 2) I have read in one datasheet there is external clock source required but in the schematic there is no pin i seen is it for another or the same.
From my understanding, you are working with the DA16200MOD. Please refer on the DA16200MOD Design Files.If you check the BOM List you can find the Oscillators:
And if you check the DA16200MOD Schematics:The DA16200MOD includes the external clock source. If you have a design with DA16200 then you would need to add the external clock source.
ak said: This is give me error CRC failed while loading.and i will check the AT command and this will not give me OK response.why this happen. i did hardware connection the PDF application schematic show's like this ckt design i did hardware connection I did RTC_wake_up2-GND, VDD_DIO2 and VDD_DIO1,VBAT,RTC wake up,rtc pwr key give 3.3V.
It is clear that you have corrupted the FW stored in the DA16200MOD. I also do not understand the reason of issuing a 100bytes erase on address 0x22000, what was the goal?I would suggest you erase the whole flash and then reflash your images. You should see on the UART0 logs a message that UART1 is initialized and after that you are able to sent AT commands:
>>> UART1 : Clock=80000000, BaudRate=115200 >>> UART1 : DMA Enabled ...
Hello Sir, Can you please tell me How to erase the flash. Yes to get only DA16200MOD chip we are going to doing our own development of WIFI module
at which pin should i connect this both crystal because i have not seen any crystal pin indication which i early attached application schematic diagram. best regard's
ak said: Can you please tell me How to erase the flash.
On the MROM menu if you write 'sflash erase' you will get the following:To erase the whole Flash you should use 'sflash erase 0 400000'
ak said: Yes to get only DA16200MOD chip we are going to doing our own development of WIFI module at which pin should i connect this both crystal because i have not seen any crystal pin indication which i early attached application schematic diagram.
Yes to get only DA16200MOD chip we are going to doing our own development of WIFI module
at which pin should i connect this both crystal because i have not seen any crystal pin indication which i early attached application schematic diagram.
DA16200MOD: Contains the external oscillators. Application Schematic for DA16200MOD:DA16200: You need to place external oscillators.Application Schematic for DA16200 QFN:Best Regards,OV_Renesas