Hello Team,
i got this module today,i just want to know this module come with build in SDK or we have to load in this after we got if not come with SDK then which SDK file we have to load. i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using UART0 as you suggest me UART0 is for debug and UART1 is for AT command) .....but after waiting some time i end the task.because it not loading..
what is the correct way to load the file and which one is correct. because i am using with HOST controller.i have RX71 controller and i want to communicate via using AT command i want to send data on IOT page using AT command and i am MQTT
protocol. Thanks and regard's AK
Hi AK,Thank you for posting your question online.
ak said: i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using
Were you able to see the progress bar on Tera Term? If there is no progress during the download please stop the procedure and try again.
ak said: what is the correct way to load the file and which one is correct.
Please refer on the UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide (renesas.com), on section 5.7 Programming Firmware Images in e2studio. and on section 5.7.3 Programming Firmware Images Using SEGGER J-LinkYou can also find pre-compiled binaries on the DA16200 Product site: DA16200 - Ultra-Low Power Wi-Fi SoC for Battery-Powered IoT Devices | Renesas
Best Regards,OV_Renesas
Hello OV Renesas, Thanks for replay, i am not using EVB DA16600 EVB Hardware Configuration. I am just using DA16200 module with rx71 microcontroller UART without EVB board can we send pre-compiled binaries images in the module.
Here i am not giving VBAT only using RX TX GND connection like RX-TX and TX-RX and GND from FTDI module to DA16200. and also tried with VBAT supply given.
here i am using UART0 is using for loading this TTL file.(i tried for UART1 also as the second image you will see that side UART1 connection is there but as you told this is for AT Command) but for both UART0 and UART1 the file issue get same.
in this image of tera term after this ttl file loading second step that i did is send the image file using YMOD but it sending the bar is not increasing.
i am using FTDI module CP2102 does this will affect for this issue because they are using FT232 IC and you have
using DSD TECH SH-U09C5 and this have IC FT232RL.or i have to take different FTDI module
and i also install drivers for the FTDI and also set the baudrate 230400.
i read on PDF there are saying that reset button should be pressed while loading the file which PIN should i connect the switch of DA16200module i attched the PDF screenshot.
or i am controlled from MCU so i connect PWR RTC KEY to VBAT as your PDF have information.
thanks and regard
AK.