Hello Team,
i got this module today,i just want to know this module come with build in SDK or we have to load in this after we got if not come with SDK then which SDK file we have to load. i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using UART0 as you suggest me UART0 is for debug and UART1 is for AT command) .....but after waiting some time i end the task.because it not loading..
what is the correct way to load the file and which one is correct. because i am using with HOST controller.i have RX71 controller and i want to communicate via using AT command i want to send data on IOT page using AT command and i am MQTT
protocol. Thanks and regard's AK
Hi AK,Thank you for posting your question online.
ak said: i have try to load this file Download_W25Q32JW_FreeRTOS.ttl & mrom_otp_lock_check.ttl by using tera term VT but it taking so much time and not loaded in the module for that i am using
Were you able to see the progress bar on Tera Term? If there is no progress during the download please stop the procedure and try again.
ak said: what is the correct way to load the file and which one is correct.
Please refer on the UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide (renesas.com), on section 5.7 Programming Firmware Images in e2studio. and on section 5.7.3 Programming Firmware Images Using SEGGER J-LinkYou can also find pre-compiled binaries on the DA16200 Product site: DA16200 - Ultra-Low Power Wi-Fi SoC for Battery-Powered IoT Devices | Renesas
Best Regards,OV_Renesas
Hello, at first SDK is load but next time i doing but it's not loading.is there have only one time loading provision have this module or any thing different step to load this SDK.thanks and regard's
AK.