DA16200MOD MQTT JSON Formate AT Command communication.

Hello Team,

                  I am going to use the MQTT Protocol, and i want to send data on JSON format is this possible. Because this i read your documents in that JSON formate AT command is only for HTTP and HTTPS protocol. if i want to use MQTT protocol then which language should we use to design the IOT page.

              and another information required i am not using RTC then RTC sensor should give ground or VDD.

because my SDK is not load in module they stuck in middle i think this is because of RTC is goes in SLEEP mode so what should we do to WAKE UP this RTC.

Best Regard's

AK.  

  • Hello ,

                  I have created IOT page on thingboard and try your command to send data it works but when i want to send my project data but it not work,


    send_command("AT+NWMQMSG={temperature:86},v1/devices/me/telemetry\r\n",53); <--->this command is working when i directly put value "temperature:86" like that, but in below code i idid using sprintf but it not working.

    just check and give me solution which data type this command support.
    snprintf is not support to RX71 so i used sprintf.


    and one more question how much delay will be required while send and get response of command because it gives me error most of the time. i also try for long delay but issue i get remain. gives me this error :-1 which is

    -1

    AT_CMD_ERR_UNKNOWN_CMD

    Unknown command



    ERROR:-1....+NWMQCL:1..:-1...52.153....OK..K-CCMP][ESS].IOT.c0:c1:c0:a6:7f:2a.2462.-80.[WPA-PSK-CCMP+TKIP][WPA2-PSK-CCMP+TKIP][WPS][ESS].Cisco-D.f8:c4:f3:94:eb:01.2457.-90.[WPA-PSK-CCMP+TKIP][WPA2-PSK-CCMP+TKIP][WPS][ESS].Foro.dc:ef:09:0d:70:70.2472.-91."

    this is my MQTT thingboard link :-

     mosquitto_pub -d -q 1 -h mqtt.thingsboard.cloud -p 1883 -t v1/devices/me/telemetry -i "clientid" -u "username" -P "password" -m "{temperature:25}"

    this red part is JSON formate data.

    #include "r_cg_macrodriver.h"
    #include "r_cg_cgc.h"
    #include "r_cg_sci.h"
    #include "r_cg_s12ad.h"
    /* Start user code for include. Do not edit comment generated here */
    #include <stdbool.h>
    #include <stddef.h>
    #include <string.h>

    #include <stdio.h> 

    /* End user code. Do not edit comment generated here */
    #include "r_cg_userdefine.h"
    #include "r_cg_s12ad.h"

    /***********************************************************************************************************************
    Global variables and functions
    ***********************************************************************************************************************/
    /* Start user code for global. Do not edit comment generated here */
    void send_command(uint8_t * const tx_buf, uint16_t tx_num);
    void delay(int t);
    void wifi_init();
    void wifi_scan();
    void LED_status();
    void LED_status_blinking();
    void LED_status_off();
    void LED_status_on();
    void LED_status_blinking_infinite();
    void mqtt_publish();
    bool check_for_string(const char* scan_result);
    void mqtt_setup();
    void LED_status_on_off();
    void wifi_status();
    void delay1(int t);

    #define size 1000
    char receive_buffer[size];
    //bool flag=0;
    //uint8_t length=0;
    MD_STATUS responsStatus;
    int i=0;
    uint16_t ADC=0;
    uint8_t j=0;
    uint16_t g_data00=0;
    //uint16_t temperature=0;
    uint16_t min_value=1500;
    uint16_t max_value=2153;
    char *scan_result;
    char mqtt_message[100];
    uint8_t INC=0;
    char array2[300];
    char array3[600];
    char command[10];

    #define BUFFER_SIZE 512 // Define an appropriate buffer size

    static uint8_t buffer[BUFFER_SIZE]; // Buffer to store received data
    static uint16_t var = 0;
    uint16_t temperature=0;
    uint16_t g_data0=0;
    int attempt = 0;

    /////Response///
    bool flag1=0;
    bool flag2=0;



    void main(void)
    {
    R_MAIN_UserInit();
    /* Start user code. Do not edit comment generated here */
    R_SCI0_Start();
    R_S12AD0_Start();


    wifi_scan();
    mqtt_setup();

    while(1)

    {
     

    sprintf(store,"%d",temperature);
    sprintf(command, "AT+NWMQMSG={temperature:%d},v1/devices/me/telemetry\r\n", store);
    send_command(command, strlen(command));
    //delay(6000);
    // wifi_status();

    // g_data0 = (uint16_t)(S12AD.ADDR0);

    // temperature = (g_data0 - 1973)*0.179;
    // sprintf(store,"%d",temperature); // Correct sprintf usage

    //sprintf(command, "%d",temperature);

    send_command("AT+NWMQMSG={temperature:63},v1/devices/me/telemetry\r\n",53);
    delay(100);

    // if(0x45==receive_buffer[2] &&0x52==receive_buffer[3]&&0x52==receive_buffer[4]&&
    // 0x4F==receive_buffer[5]&&0x52==receive_buffer[6]&&0x3A==receive_buffer[7]
    // &&0x2D==receive_buffer[8]&&0x36==receive_buffer[9]&&0x33==receive_buffer[10]
    // &&0x34==receive_buffer[11])
    // {
    // send_command("AT+LEDCTRL=1,off\r\n",18);
    // delay(50);
    // }
    // sprintf(command, "AT+NWMQMSG={temperature:%s},v1/devices/me/telemetry\r\n", command);
    // send_command(command, strlen(command));
    // delay(100);
    //mqtt_publish();

    }


    /* End user code. Do not edit comment generated here */
    }

  • Hi AK,

    Thank you for the reply.
    IF you are trying to connect to AWS Server via MQTT, please refer here: DA16200 DA16600 Getting Started with AWS IoT Core (renesas.com)
    You will need the AWS IoT Reference for FreeRTOS SDK or the AWS IoT ATCMD Image for FreeRTOS SDK which can be found on the DA16200/DA16200MOD/DA16600MOD product pages under Software Downloads;

    Please follow the ReadMe files on how to integrate the AWS features into the FreeRTOS SDK.

    If you are still facing issues, please attach a logic analyzer on the UART/SPI lines being used for AT command transport and share the capture with us.
    We would also like the full UART0 log files.

    Best Regards,
    OV_Renesas

  • hello,

                Yes i will try with this SDK images.

    Best Regard's
    AK

  • Hello,

                        Without using AWS freertos SDK it works. there is some code logic issue which i resolve it and i successfully hit the data on thingsboard IOT page i use MQTT protocol.


    best regard's
    AK.