DA16200 not probed in linux

Hi Team,

My platform is TI AM62x processor . Linux kernel is 6.1.33, driver version is  v5.2.1.2, use the sdio interface 

After I insert the driver, the initialization function returns 0, indicating that there is no error in initialization.

But the probe function did not run . What could be the reason?

Parents Reply Children
  • Hi St,

    Thank you for the replies.
    Yes, for the UART0 you will need 230400 Baudrate. This is mentioned on UM-WI-056 DA16200 DA16600 FreeRTOS Getting Started Guide (renesas.com), on section 4.4.1 Configuring DA16200/DA16600 Serial debug Interface.

    The UART log after startup is as follows:

    I have a question to confirm: Is the Flash erase operation mentioned in the Start Guide mandatory?

    Based on the UART0 logs you are using a really old SDK version (which is not supported0 and should have been erased in order to use the Linux Driver.
    The ThreadX SDK has not been supported since 2020-2021. We officially only support the FreeRTOS SDK v3.2.x.x , the Matter SDK and the Linux Driver.

    Please follow the steps on 4.1.1 How to Erase Flash and make sure you issue the following:

    sflash erase 0 400000

    In order to erase the whole contents of the Serial Flash. You can verify this with the sflash read command. 

    After erasing the Flash please follow the procedure again.

    Best Regards,
    OV_Renesas

  • Hi,

    1. After erasing the Flash, do we need to rewrite the SDK into it? Currently, after erasing the Flash, the system reports a "Boot Err" during startup.

    2. The RZ/G2L Linux System mentioned in the Starter Guide is the system build environment you are using, correct? If we use our own Yocto environment, which configurations do we need to port?

    3. After following the kernel configuration steps in the documentation, I compiled rswlan.ko. Although the system indicates that the firmware has been loaded after module insertion, the device's probe function still hasn't been executed. 

    As shown below, the driver successfully registered DA16200_sdio_fw_download and DA16200_sdio, with both functions returning rtn as zero, indicating that the registration was successful. However, the probe function was invoked when registering sdio_fw, but it was not called when registering sdio.

  • Hi ST,

    Thank you for the reply.
    I am checking on this with the Wi-Fi Support Team and I will get back to you as soon as possible.
    I have also reached out to you directly, please check your PM.

    Best regards,
    OV_renesas

  • Hi ST,

    Apologies for the delay.
    Please find the answers from the Wi-Fi Support Team:
    1. No. You do not need to rewrite an image. TO run the DA16200 with the Linux driver, the entire contents of the flash memory should be erased first. The linux driver will download the firmware to the DA16200.

    2. Without the details of the custom Yocto, we cannot provide exact configurations that need to be ported to a custom Yocto.

    3. It seems that the driver cannot get the MAC address from DA16200. We think that the status of the CD pin should be checked to see if it is low or not. To proper operation, the CD pin should be low. Please refer to the user manual on section 4.7.1
    UM-WI-059 DA16200 DA16600 Linux Driver Getting Started Guide (renesas.com)

    If you have any further questions, please let us know. Please also check your Private Messages and share with us some details there as well.

    Best Regards,
    OV_Renesas